I have configured a TMS570LS1224-based LaunchPad XL2 for a PLL1 frequency of 80 MHz. Most clocks in the system use PLL1 as a source, but after initialization they still all are 16Mhz, the frequency of the external oscillator. PLL1 is enabled, and its valid bit is set CSVSTAT. Any of oscillator clock, GLK, RTI base, VCLKA1, VCLKA2, VCLKA4 routed to ECLK through CLKTEST show 16 MHz, but PLL1 out put is 80 MHz as intended. Using other clock sources (e.g. HF LPO) shows the frequency of the selected clock source on ECLK.
Thanks and Best Regards,
Daniel Marmier