Hello,
We have two boards, one with a TMS570LC4357 in SLAVE MibSPI mode. They are linked with a SPI bus, (One clock, one SIMO, one CS).
The data arrives on TG2 because CS1 is activated.
The master board send always the same pattern (1, 2, 3, ... 22) at 1.25 MHz every 1 ms.
When we power on the slave board, if the first reception coming from the master is correct, every thing will be OK till the power off. If the first reception is not correct (i.e. data not equal the the sent message), everything goes wrong till power off or CS1 put to ground/+5V manually.
If the clock wire is manually switched off/on, the reception will be corrupted as described above.
Verification of the TG2 (0XFF0C0200) received data is done in CCS7 in memory browser.
HCG project :
Regards,
Alain.