Tool/software: TI C/C++ Compiler
Hi I am getting this problem
Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 7.0.48.0)
Actually I am testing code for low power mode of tms570ls0432 controller .
#ifdef FLASH_BANK_SLEEP
flashWREG->FBFALLBACK = 0x00000000U
| (uint32)((uint32)SYS_SLEEP << 14U) /* BANK 7 */
| (uint32)((uint32)SYS_SLEEP << 0U); /* BANK 0 */
#endif
systemREG1->CSDIS = 0x00000000U
| (uint32)7U << 3U
| (uint32)1U <<1U;
flash1 = (uint32)systemREG1->CSDIS & (0xFF);
while(1) {}
Here i am following the TRM . I programmed first flash bank to sleep and then clock source disable register .. and i was monitoring the flash1 variable in watch window .
AND after that i am getting this error ....
How to come out of this !!
Thank you .