Other Parts Discussed in Thread: TMDX570LC43HDK, HALCOGEN, , TCAN4550-Q1
Hello,
I have the TMDX570LC43HDK and am trying to confirm the basic operation for the board.
I had wanted to check the basic LED demo, and then use the CAN demo to read CAN messages on a basic CAN bus.
However, the Hercules Safety Demos will not run. Is this the same issue related to the change in board driver chip? Something about the XDS110 or the XDS100v2 Emulator looking for a non-existent FTDI chip?
So my alternate attempt: launch CCSv7.4.0.00015 and try a different CAN example. However, I can't locate any device documentation for the TMS570LC43, (or any TMS570) using the Resource Explorer, so what now?
I have then launched the HALCoGen tool for the TMS570LC43x, I open up examples, but I just get a link to a bunch of .c files, with no clear means of importing them into CCS, or integrating them into a HALCoGen project.
I just want to be able to load an example into an IDE (and associated configuration files, as necessary), compile the example, download it to the target board, and see it work.
I see that TI has created all these amazing tools, and provided development hardware as well, but the specific device I want to use is not listed.
I see the intro video covers loading an example, compiling the example, loading it to a target, and then entering debug mode, with all the familiar debugging tools, register views, breakpoint views, etc.
Is this device still supported? What am I missing? Why is there no simple means for loading an example, compiling, loading, and debugging?
Should I just switch to a different solution? I am looking for a development target with minimum 3x CAN FD and 10/100 Ethernet capability and IEC61508 SIL 3 design capability.
What am I missing?