Other Parts Discussed in Thread: HALCOGEN
Hello,
I am very new to the Hercules platform. I am in the middle of trying out the Hercules for a prototype which involves measuring 60Hz zero crossings. I have done this before with slower 8-bit controllers with no problem but I'm having a problem figuring out how to do it with this chip. Is there a way that I can get the N2HET timing system to go slow enough that the Loop Resolution will be about 10ms? If I understand correctly, that would be how I would have to do this. On 60Hz, pulses would come at every zero, so they are ~9 ms apart from one another, and the timer system would need to see two pulses within the same loop time for it to know the difference between them, correct?
Sorry if this is a dumb question. I'm trying to figure it out with HALCoGen, but the interface is all distorted on my computer and it makes it hard to see what is really there and what isn't.
Thanks