so there is an internal mapping from NHET1 to mibspi for the trigger. can I setup a NHET1[8] then as an edge capture and if there is a LOW on the NHET1[8] pin/pad it will somehow cause the MIBSPI to be triggered?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
so there is an internal mapping from NHET1 to mibspi for the trigger. can I setup a NHET1[8] then as an edge capture and if there is a LOW on the NHET1[8] pin/pad it will somehow cause the MIBSPI to be triggered?