Other Parts Discussed in Thread: HALCOGEN
Hercules Friends and Family,
A few questions from our customer; any input welcomed:
If I only need to use the MIBSPI4CLK pin as a GIO instead of a functional one, do we still have to Enable Driver Compilation?
NOTE: We are only running in 3-Pin Mode.
2. If I do have to enable the associated driver, but still only need to use the MIBSPI4CLK pin, does it make any difference if I configure the port for SPI Compatibility Mode or MIBSPI mode? I realize that if the other device we are communicating with only supports standard SPI that could change the answer but we are just trying to get familiar with the new system and understand best practices.
3. In cases where a GIO signal is needed and two choices can be made (i.e. because both resources are available in the design), is there a recommended best practice? For example, either MIBSPI5SIMO[3] or DMM_DATA[11] could be used as the GIO as shown:
4. It would be very beneficial, if it is not already available, to have a concise location/screen in HALCoGen that illustrates all the possible solutions for mapping a required GIO to a module/subsystem? See #3 above.
5. Is there any general, as opposed to specific cases, TI produced Best Practices documentation available (i.e. without having to filter through the TI E2E Community site)?
(#5 can be addressed with TI Training, as noted)
Again, comments welcomed.
TY,
CY