Tool/software: TI C/C++ Compiler
I'm using the LCF file with TI's compiler in Code Composer to generate a CRC value for comparing against the value generated by the safety library's "SL_CRC_Calculate" function. The two values are not matching due to the upper and lower words being swapped. Document "spna235" says that this is an intended feature of the TMS570_CRC64_ISO algorithm. Is there an algorithm I can use witch does not have this feature, or another way to correct the problem (besides swapping the byte order in code before comparing the values?)
Thank You