Tool/software: Code Composer Studio
Dear All,
I am trying to write an integer to EEPROM @ BLOCK_NUMBER = 0x1. But I can not see the writen value on Memory Viewer.
Whay maybe the problem ?
Thanks.
/* USER CODE BEGIN (0) */ #include "ti_fee.h" /* USER CODE END */ /* Include Files */ #include "sys_common.h" /* USER CODE BEGIN (1) */ uint16 Status; uint8 SOC; Std_ReturnType oResult=E_OK; unsigned char read_data[100]={0}; unsigned int BlockOffset, Length; unsigned char *Read_Ptr=read_data; int sayac=0; void delay(void) { unsigned int dummycnt=0x0000FFU; do { dummycnt--; } while(dummycnt>0); } /* USER CODE END */ /* USER CODE BEGIN (2) */ /* USER CODE END */ void main(void) { sayac++; printf("BEKLE\r\n"); SOC = 66; unsigned int BLOCK_NUMBER = 0x01; TI_Fee_Init(); do { TI_Fee_MainFunction(); delay(); Status=TI_Fee_GetStatus(0 ); } while(Status!= IDLE); printf("BEKLE\r\n"); sayac++; TI_Fee_WriteAsync(BLOCK_NUMBER, &SOC); do { TI_Fee_MainFunction(); delay(); Status=TI_Fee_GetStatus(0); } while(Status!=IDLE); sayac++; printf("BEKLE\r\n"); TI_Fee_WriteSync(BLOCK_NUMBER, &SOC); /* Read the block with unknown length */ BlockOffset = 0; Length = 0xFF; oResult=TI_Fee_Read(BLOCK_NUMBER,BlockOffset,Read_Ptr,Length); do { TI_Fee_MainFunction(); delay(); Status=TI_Fee_GetStatus(0); } while(Status!=IDLE); sayac++; printf("BEKLE\r\n"); /* Invalidate a written block */ TI_Fee_InvalidateBlock(BLOCK_NUMBER); do { TI_Fee_MainFunction(); delay(); Status=TI_Fee_GetStatus(0); } while(Status!=IDLE); sayac++; printf("BEKLE\r\n"); /* Format bank 7 */ TI_Fee_Format(0xA5A5A5A5U); sayac++; printf("BEKLE\r\n"); while(1); /* USER CODE BEGIN (3) */ /* USER CODE END */ }