• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » Hercules™ Safety Microcontrollers » All Tags » EMIF
Share
Hercules™ Safety Microcontrollers
  • Forum
  • E2E Wiki

Browse by Tags

Hercules™ Safety Microcontrollers

Welcome to the Hercules™ Safety Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
EMIF
  • CortexR4
  • delay between cycles
  • example code
  • gio
  • HALCoGen
  • HDK
  • heap
  • MPU
  • Normal Mode
  • nWE
  • RM48
  • RM48L950 HDK
  • RM48L952ZWTT
  • safety
  • SDRAM
  • tms570
  • TMS570LS
Related Posts
  • Forum Post: EMIF Interface to 256K 16-bit SRAM

    Tony Morrell Tony Morrell
    Hi, The Technical Reference Manual Figure 10-8 in section 10.3.1.1 describes the EMIF interface to an 8-bit RAM. Here A[18:0] and EMIFBADD[1:0] are used to form the SRAM 21-bit address A[20:0]. We wish to interface to a 16-bit SRAM (CY7C1041CV33) which allows 16-bit data access as well as high...
    on Oct 12, 2010
  • Forum Post: Re: EMIF Interface to 256K 16-bit SRAM

    Jean-Marc Mifsud Jean-Marc Mifsud
    Tony, To connect an external 16bits memory with BLE/BHE for 8bits accesses, please follow this recommandation: EMIFADD[16:0] to SRAM_ADD[17:1] EMIFBADD1 to SRAM_ADD[0] EMIFDQM0 to SRAM_BLE EMIFDQM1 to SRAM_BHE The EMIF has to be programmed as following: Select Strobe = 0 Enhanced Wait = 0...
    on Oct 12, 2010
  • Forum Post: External RAM

    Livio Franchin Livio Franchin
    In our project we need to use an external static ram to store data in safety mode. (about 2Mbytes) Reading the safety manual of TMS570 I found that is not possible to use the external memory interface (EMIF) for safety application because it is not a safety critical device component. How can...
    on Feb 23, 2011
  • Forum Post: EMIF Unused Pins for GIO

    Tony Morrell Tony Morrell
    Hi, The TRM does not say that the EMIF pins can be used for GIO. Can you please confirm that this is the case, EMIF pins do not have GIO capability. Regards, Tony.
    on Apr 19, 2011
  • Forum Post: Re: TMS 570 MDK Parallel I/O

    Pratip Kumar Pratip Kumar
    Rob, Does this answer your question ? Click on verify Answer if your questioin is answered. - Pratip
    on Dec 30, 2011
  • Forum Post: TMS570 and example code for setting up an extarnal SRAM.

    Magge Ericsson Magge Ericsson
    Hello TI, I wonder if you have an example code/project for setting up EMIF for an external SRAM (ISSI IS61WV102416BLL) for the TMS570? Best regards Magnus
    on Jan 3, 2012
  • Forum Post: RM48 EMIF Module in Halcogen

    Vanderwegen Martin Vanderwegen Martin
    Hi, I'm trying to use the EMIF module of the RM48 using halcogen in order to use the 8MB SDRAM. To configure it I've done the following steps: 1. Create a RM4x, TMDXRM48HDK project. 2. Set EMIF driver in Driver Enable Tab 3. Enable EMIF SDRAM in EMIF General 4. Set EMIF SDRAM...
    on Apr 5, 2012
  • Forum Post: How to access TMS570LS31 HDK SDRAM?

    Takashi TAKATORI Takashi TAKATORI
    Hi, I got TMS570LS31x Hercules Development Kit, and want to use the external 8MB SDRAM. But, it seems that I can't access SDRAM. Is there any initialization step to use SDRAM? I made TMDX570LS31HDK project by HALCoGen(2.09.001) and "Generate Code" default settings. I added some callback...
    on Apr 14, 2012
  • Forum Post: Re: How to access TMS570LS31 HDK SDRAM?

    Jean-Marc Mifsud Jean-Marc Mifsud
    Takashi, The SDRAM on the HDK is accessible via the EMIF Module. There is another thread on the forum with an example at the following link http://e2e.ti.com/support/microcontrollers/hercules/f/766/t/180728.aspx Please have a look and let me know. Regards, Jean-Marc
    on Apr 16, 2012
  • Forum Post: RM48 - EMIF - Async Connection to FPGA - 3rd nWE pulse!

    stomp stomp
    Hi, I have a RM48 950 on the HDK. I have connected the EMIF to a Xilinx FPGA and, as a starting point, scoped the signals when I do a basic EMIF write from RM48 to FPGA. I am writing to a FIFO and are not using any addressing scheme, other than relying on BA[1:0] from the RM48 to determine the upper...
    on May 15, 2012
  • Forum Post: EMIF - Delay between cycles

    Petr Burian Petr Burian
    Hi, I writing to ask you what is minimal delay between individual emif read/write cycles. I used the EMIF (async.;16bit; emif clock 90MHz). I exploit an access through 64-bit pointer. If I perform two emi read/write cycles immediately successive, emif produces four read/write 16-bit cycles but...
    on Sep 3, 2012
  • Forum Post: Use EMIF

    Pablo Cottens Pablo Cottens
    Hello. I'd like to use the EMIF connected to a SDRAM (2M) instead of the internal RAM of the microcontroller (256k). How could I achieve that? Is it possible to determine all of this on boot up, or do I have to write a piece of code inside my application to start the EMIF? Do I have to write...
    on Nov 1, 2012
  • Forum Post: How to make SDRAM work in Hercules HDK

    Michael Enggaard Pedersen Michael Enggaard Pedersen
    Hello, I am trying to get the SDRAM to work on our Hercurles HDK. I am using HALCodGen to generate the code. From the schematics (and verified on the board) I can see that the SDRAM is a IS42S16400F-7BL. From the data-sheet I have looked up the timing and done the following in Halcogen: 1: Set...
    on Jan 7, 2013
  • Forum Post: RE: EMIF - Delay between cycles

    Christian Herget Christian Herget
    Hi Zhaohong, Do I understand you right, that if the MPU is configured to Strongly Ordered we will have 12 cycle delay on the buses plus 12 cycles delay in the EMIF for burst access, which calculates to a total delay of 24 cycles? Thanks, Christian
    on Jan 15, 2013
  • Forum Post: external RAM with EMIF

    enrico terraneo enrico terraneo
    Hi all, I'm using TMS570LS3137 with CCS v5. My project has two external RAM connected to TMS570 by EMIF. I would like to use the two external RAM in a redundant configuration , so as to increase the safety of data stored. I'm again evaluating two possible cases of How to use the external...
    on Jan 23, 2013
  • Forum Post: .bss -> EMIF SDRAM

    Pierre Negre Pierre Negre
    Hi! I want to run .bss section on the SDRAM of the RM48 board. The uC is RM48L952LWTT. The SDRAM is ISSI IS42S16400F http://www.issi.com/pdf/42S16400F.pdf . Softs : HALCOEN v3.05 and CSSV5 What i've done : /* Linker Settings */ --retain="*(.intvecs)" /*-----------------------------...
    on Mar 25, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use