• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » Hercules™ Safety Microcontrollers » All Tags » TMS570
Share
Hercules™ Safety Microcontrollers
  • Forum
  • E2E Wiki

Browse by Tags

Hercules™ Safety Microcontrollers

Welcome to the Hercules™ Safety Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
TMS570
  • ADC
  • CCS
  • CCS4
  • compiler
  • CRC
  • DCAN
  • DCAN communication
  • DMA
  • DMA TMS570
  • ECC
  • EMIF
  • ESM
  • FIQ
  • Flash API
  • Flash Programming
  • FlexRay
  • FPU
  • gio
  • HALCoGen
  • HDK
  • HET
  • Initialization
  • interrupt
  • interrupts
  • JTAG
Related Posts
  • Forum Post: How do we configure the PLL on the TMS570LS series devices?

    S Tsuei S Tsuei
    The configuration of the main PLL and clock wrapper is controlled by two registers, PLLCTL1 (offset 0x70) and PLLCTL2 (offset 0x74) in the System module. Programming these two registers selects the operating mode, frequency, reset behavior on PLL slip or oscillator fail. . PLLCTL1 register...
    on Mar 3, 2010
  • Forum Post: What are the reset requirements?

    S Tsuei S Tsuei
    Power-on-reset: When either of the core (1.5V nom) or I/O (3.3V nom) supply voltage is detected out of regulation, the power on reset input pin (nPORRST) must be asserted by the external power supply monitoring circuitry for at least 1 ms. (Core supply min required and max allowed are 1.35 V and 1...
    on Mar 4, 2010
  • Forum Post: What kind of oscillator/crystal can be used?

    S Tsuei S Tsuei
    A few requirements apply. When using a crystal/resonator across OSCIN and OSCOUT, the resonator/crystal frequency should be within 5-20 MHz range. When using an external clock source driving OSCIN (OSCOUT unconnected) the clock signal should be toggling 0-1.5 V. Please refer to the TMS570LS series...
    on Mar 4, 2010
  • Forum Post: What are the available clock sources and domains? What registers are used to map a selected clock source for a particular domain?

    S Tsuei S Tsuei
    The clock sources and domains are managed by the Global Clock control Module (GCM). The clock domain output signals generated (from the selected clock source input) by the GCM are used to clock the various modules on the device. GCM also controls the enabling and disabling of the clock sources and domains...
    on Mar 7, 2010
  • Forum Post: How are error conditions handled?

    S Tsuei S Tsuei
    The various error conditions on the device are managed by the Error Signaling Module (ESM). The severity level of the error determines how the error is handled. The severity level is device specific and is implemented by mapping each of the device error signals to the appropriate group of error/interrupt...
    on Mar 10, 2010
  • Forum Post: Re: Stack usage and function call information in cl470.exe

    A Arora A Arora
    The code generation tools come with a Stack Depth Profiler. If I get your question right, then this may be able to help you. This tool (sdp470.exe) can be found in your CCS installation directory. For CCSv4 users the default installation location for the compiler tools is: \Program Files\Texas Instruments...
    on Mar 25, 2010
  • Forum Post: Jump to App from boot

    Anil Mathews Anil Mathews
    I have a very trivial boot code[just a PLL init and checking if a valid app is present]. How can I make a jump to the App. Can some one share how you jump from boot to App.
    on Apr 13, 2010
  • Forum Post: EMV/EMC and TMS570LS20216S

    Marcus Frech Marcus Frech
    Is there a kind of hardware design guideline or reference design with consideration of EMV/EMC for the TMS570LS20216S available?
    on Apr 16, 2010
  • Forum Post: Re: Jump to App from boot

    John Hall John Hall
    One way I do this is hard code an address to a symbol in the command linker file for the boot code. /* SPECIFY THE SYSTEM MEMORY MAP ********************************************/ MEMORY { RAM (RWX) : origin=0x08000000 length=0x00001100 STACK (RW) : origin=0x08001100 length=0x00001400 } /******...
    on Apr 22, 2010
  • Forum Post: Re: Jump to App from boot

    John Hall John Hall
    Here is the code used for the boot code. Note: The function being called, Init_code() will be decorated in TI's COFF format as $Init_code which is what the symbol is referred to in the command linker file. Using EABI format, there is no decoration and the symbol would be Init_code in the command...
    on Apr 23, 2010
  • Forum Post: Re: can i use j-link in ccs v4.1 to debug tms570ls20216?

    sowa sowa
    You can also use JTAGjet-470, JTAGjet-570 or JTAGjet-CCS from Signum Systems. They all support CCStudio 3.3 and 4.x. See: http://www.signum.com/jtagjet.htm
    on May 4, 2010
  • Forum Post: Re: Can 3rd-party JTAG emulator be connected to J1 on TMS570 Microcontroller USB Kit?

    Anthony Vaughan Anthony Vaughan
    The TMS570 USB Stick features an on board XDS100v2 JTAG emulator. The on board XDS100v2 is the primary solution for JTAG connectivity to enable debug and flash programming on this piece of hardware. The J1 pads on the bottom of the board that provide access to the TMS570 JTAG signals are intended for...
    on Jun 29, 2010
  • Forum Post: Re: FlexRAY for the TMS 570

    Roy Haley Roy Haley
    We do not have specific TMS570 FlexRay application notes, but there are several E-Ray application notes available on the Bosch AE webpage ( http://www.semiconductors.bosch.de/en/20/flexray/flexray.asp ). The TMS570 uses the Bosch AE E-Ray (Flexray) module. FlexRay drivers for TMS570 are available...
    on Jul 1, 2010
  • Forum Post: TMS570 TRM/User's Guide, Datasheet, and Errata are now available.

    S Tsuei S Tsuei
    Documentation for TMS570LS series devices is available: TMS570 series Microcontroller Technical Reference Manual/User's Guide (SPNU489) http://focus.ti.com/lit/ug/spnu489c/spnu489c.pdf TMS570 series Microcontroller Datasheet (SPNS141): http://focus.ti.com/lit/ds/spns141f/spns141f.pdf TMS570 series...
    on Jul 16, 2010
  • Forum Post: TMS570 ESM

    Richard Burke Richard Burke
    The TMS570 Technical Reference Manual contains a section on the Error Signalling Module where it talks about groups and channels. There are some references to Group 2 channels 6, 8, 10 and 12 in the document. Where are the channels for each group defined? Thanks
    on Jul 30, 2010
  • Forum Post: Re: 570 solutions for automated serial flash programming

    John Hall John Hall
    Jeff, I have never used an ICT tester per se so I cannot comment on how to set one up for this. Our current TMS570/470 customers either use an offline programming solution or use their own methods for programming the devices in circuit with or without their own proprietary boot code.. There are...
    on Aug 3, 2010
  • Forum Post: Re: 570 solutions for automated serial flash programming

    John Hall John Hall
    Jeff, They are in the process of adding their support for the TMS570 devices which should be done in the next couple of months. As soon as they are finished and we have validated their solution, it will be added as a 3rd party tool link on the page.
    on Aug 3, 2010
  • Forum Post: Phantom interrupt vector

    Richard Burke Richard Burke
    The TMS570 has a phantom interrupt vector but I can find no reference in the technical reference manual as to why or when it is called. Is this vector called when there is no entry for an interrupt in the CHANMAP registers?
    on Aug 6, 2010
  • Forum Post: TMS570 MCU Development Kit example application

    Richard Burke Richard Burke
    We have purchased a number of the TMS570 MCU Development Kits which come loaded with an application that demonstrates the functionality of the board. However the source code for this application does not appear to be supplied on the CD that comes with the kit. Is there a link for the source code?
    on Aug 10, 2010
  • Forum Post: TMS570 Interrupt priorities

    Richard Burke Richard Burke
    It is my understanding that the TMS570 effectively has only two interrupt priorities, IRQ and FIQ. Whilst the CHANMAP mechanism provides a way to rank interrupts in priority order, this only applies when two interrupts are pending and an IRQ interrupt cannot be interrupted by a higher priority IRQ interrupt...
    on Aug 12, 2010
  • Forum Post: Re: Recommended initialization procedure for TMS570 Microcontrollers.

    Jeff Stafford Jeff Stafford
    Where can I find example code that uses the recommended 570 initializations as described in SPNA119? It would be helpful to add a link to the Application Report download page ( http://focus.ti.com/mcu/docs/litabsmultiplefilelist.tsp?sectionId=96&tabId=1502&literatureNumber=spna119&docCategoryId...
    on Aug 12, 2010
  • Forum Post: CCS Debugger (XDS510 USB) erases all memory

    Richard Burke Richard Burke
    We are using CCS4 and the Spectrum Digital XDS510 USB JTAG debugger. When debugging an application, the whole of flash memory is erased. This makes it difficult to debug applications that require a bootloader or calibration memory. Is there any way to erase a range of addresses rather than all of...
    on Aug 13, 2010
  • Forum Post: Clock Cycle Profiling

    Lucas Wendling Lucas Wendling
    I'm looking for a fairly simple method to count clock cycles that a particular block of code takes to execute on a TMS570. I'm debugging through JTAG on the target (with a Spectrum Digital XDS510 emulator), however, the profiling options I've seen for CCS v4 don't seem to be enabled ...
    on Aug 23, 2010
  • Forum Post: Re: FLASH API problem

    John Hall John Hall
    After a further discussions with Walt off forum, we have determined the issue was with the delay parameter he was passing to the Flash API routines. He was setting the PLL to have a 100MHz clock which should have a 50 for the wait value, but he was passing a value of 8. Once he corrected this value,...
    on Sep 2, 2010
  • Forum Post: Re: Running FLASH API from RAM

    John Hall John Hall
    Hello Walt, Here is an example command linker file that would put the Flash API in flash but run it from RAM. Your code would still be responsible to copy the code from Flash into RAM, but it defines the FlashApi_xxx symbols to know where the Load and Run locations are. /****************...
    on Sep 7, 2010
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use