• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » Hercules™ Safety Microcontrollers » All Tags » TMS570LS20216
Share
Hercules™ Safety Microcontrollers
  • Forum
  • E2E Wiki

Browse by Tags

Hercules™ Safety Microcontrollers

Welcome to the Hercules™ Safety Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
TMS570LS20216
  • 510USB
  • CCS
  • ECC
  • Emulator JTAG
  • example code
  • Flash Programming
  • HALCoGen
  • HET
  • IAR
  • Initialization
  • interrupt
  • interrupts
  • JTAG
  • MCBTMS570
  • mibspi
  • NHET
  • programming
  • RTI
  • SPI
  • TMDX570LS20SUSB TMS570 TMS570LS20216
  • tms570
  • TMS570 application development
  • tms570 compiler
  • TMS570LS
  • TMS570LS2x
Related Posts
  • Forum Post: Problems generating a RTI interrupt

    Ralf Eckhardt Ralf Eckhardt
    Hello, I'm using an MDK CCS4.x and HalCoGen 2.09 (Please visit the site to view this file) I want to generate a periodic interrupt with the RTI Compare 0 Module. I have provided all the settings in the Halcogen the RTI and the interrupt manger, but I still get no RTI Interrupt. What do...
    on Jul 27, 2011
  • Forum Post: Re: Problems generating a RTI interrupt

    Ralf Eckhardt Ralf Eckhardt
    Hello all, the problem is solved ! Prahap, your hint hrelped, but this was not all : In Halcogen, the vector interrupt in the int hadler for IRQ needs to get set in interrupts and in addition the VFP in the CortexR4F. See examplex enclosed. BR Ralf (Please visit the site to view this...
    on Jul 28, 2011
  • Forum Post: Re: TMS570 Board error

    Christian Herget Christian Herget
    Ranjith, as far as i understood from your posts, you are not able to Erase the flash memory of the TMS570 anymore. This can happen if you put the CPU into sleep mode for example. I did not verified your PLL settings you made in the nowFlash GUI, why do you need them? NowFlash should work without...
    on Sep 27, 2011
  • Forum Post: Error: Instruction requires VFP or NEON support.

    Gowdham Natarajan Gowdham Natarajan
    Hi, I am using TMDX570LS20SUSB controller. In CCS, i am trying to enable and initialize the floating point option. But it shows error as, PROBLEM 1: mrc p15, #0x00, r0, c1, c0, #0x02 orr r0, r0, #0xF00000 mcr p15, #0x00, r0, c1, c0, #0x02 mov r0, #0x40000000 fmxr fpexc, r0 [E0002] Instruction...
    on Oct 17, 2011
  • Forum Post: Where are the OTP values with ECC errors for TMS570LS20216?

    Juan Martinez Juan Martinez
    I have read in the forum that there are OTP values with 1-bit and 2-bit ECC errors, but I can't find them in the TRM or data sheet for the TMS570LS20216. Where are they located? Do they exist for this board? -Juan
    on Dec 2, 2011
  • Forum Post: hetGetTimestamp always returns 0

    Kevin Spharler Kevin Spharler
    What are the pre-requisites for using the HET's timestamp function? I've tried all kinds of things but I have yet to get hetGetTimestamp to return anything but 0 to me. Thanks, --Kevin
    on Dec 13, 2011
  • Forum Post: Re: little endian software migrate to tms570

    Pratip Kumar Pratip Kumar
    Hi Martin, First of all sorry for the delayed reply. The device TMS570LS20216 is big endian only device and the code you have needs to be recompiled for executing it on this target. We have a device RM48x which is little indian and has all the h/w peripherals supported on TMS570LS20216. You may consider...
    on Dec 30, 2011
  • Forum Post: Web Applications in TMS570

    karthick durai karthick durai
    We plan to buy a TMS570 HDK kit. What are the sample applications using Internet will be available in the CD?
    on Jan 10, 2012
  • Forum Post: IAR Floating point code options

    Gowdham Natarajan Gowdham Natarajan
    Dear all, I am working on TMDX570LS20SUSB development board with IAR compiler. In this i am facing a scenario during Floating point implementation as FIQ / IRQ interrupt. When i define the ISR with the attributes ( __fiq __arm ), the following codes which are marked as red, inserted automatically...
    on Jan 12, 2012
  • Forum Post: Re: MIBSPI5 working

    Christian Herget Christian Herget
    Hi Bindu, Yes it is possible to configure the MIBSPIP5 to behave as MIBSPI1 or MIBSPI3. With the help of the register SPIPC0 (SOMIFUN[7:0] and SIMOFUN[7:0]) you can configure the function of the MISO and SOMI pins as normal GPIO pins or as SPI functional pins. The SPIPMCTRL Register can be used...
    on Feb 20, 2012
  • Forum Post: could not read cp15

    edna salazar edna salazar
    hello, Im work on MCBTMS570 and y trying to download a program into the memory flash but I have the following problems/ Could not read CP15 - ERROR: Could not start CPU core. (ErrorCode: -1) I can see on my board led1 and led4 turn on FT1_error and ft2 error , I don't know how to solve...
    on Mar 20, 2012
  • Forum Post: Failed to erase flash

    J Yin J Yin
    Hi, I am working on TMS570 20216. After tried to copy flash block from 0x00080000 to 0x00000000, the error occur: CortexR4: Flash Programmer: Error initializing device. CortexR4: Flash Programmer: Error erasing Flash memory. CortexR4: Flash Programmer: Error erasing Bank 0, Sector 0. Operation...
    on Apr 12, 2012
  • Forum Post: RE: TMS570LS20216

    suresh B91852 suresh B91852
    Hi, As the device TMS570LS20216 utilizes Big endian i want to get it clarified on interface of Address and Data.. where to connect what like D0-----to D30 or D31...etc.. and address. similarly for other things need to be taken care in schematics level. please explain with illustration
    on Jul 26, 2012
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use