• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » MSP430™ Microcontrollers » MSP430 Ultra-Low Power 16-bit Microcontroller Forum » MSP 430F2274 receiving Interrupt not triggered
Share
MSP430™ Microcontrollers
  • Forum
  • Announcements
  • E2E Wiki
Options
  • Subscribe via RSS
MSP430 Resources
  • MSP430 Product Folder
  • MSP-EXP430G2 - MSP430 LaunchPad Value Line Development kit
  • MSP430 Getting Started Guide
  • MSP430 Microcontroller Projects
  • More Resources >
  • Forums

    MSP 430F2274 receiving Interrupt not triggered

    This question is not answered
    DAC CAD
    Posted by DAC CAD
    on Apr 01 2012 16:32 PM
    Prodigy60 points

    Hello;

    I am running the MSP430F2274 (CC2530 ZNP mini kit) examples for communication through UART. I have an FTDI USB 3.3V cable with USB on one end and UART RX and TX on the other. The hyper terminal and the receiving java program correctly receives the value from the MSP device. The MSP device is running in a loop and transmitting A-Z and this part of the functionality executes without any problem.

    When I transmit from the java program the MSP interrupt for reception is not triggered. The problem then should lie in the java program / hyper terminal i.e on the transmitting side or the code of the MSP device on the receiving side. To eliminate the transmitting side, I looped back the RX and TX connections (on the UART side) of the FTDI's USB cable. The characters transmitted was correctly received on the console. This probably indicates that transmission till the MSP device is okay, which eliminates cable, connections (Rx/Tx) and settings. The transmission from the device was earlier tested indicating the baud rate and 8N1 to be correct on both sides. I dont know why the interrupts are not being triggered.

    In the program shown below, which was tested on the device . If I change  IE2 |= UCA0RXIE ; to  IE2 |=  UCA0TXIE;, then the output prints Hello World.

    The initializing code for UART is working on the kit. Any ideas, what mistake, am I committing? any additional set up required?

    const char string1[] = { "Hello World\r\n" };
    unsigned int i;

    void main(void)
    {


    WDTCTL = WDTPW + WDTHOLD; // Stop WDT
    BCSCTL1 = CALBC1_1MHZ; // Set DCO
    DCOCTL = CALDCO_1MHZ;
    P3SEL = 0x30; // P3.4,5 = USCI_A0 TXD/RXD
    UCA0CTL1 |= UCSSEL_2; // SMCLK
    UCA0BR0 = 104; // 1MHz 9600
    UCA0BR1 = 0; // 1MHz 9600
    UCA0MCTL = UCBRS0; // Modulation UCBRSx = 1
    UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
    IE2 |= UCA0RXIE ; // Enable USCI_A0 RX interrupt + UCA0TXIE

    __bis_SR_register(LPM0_bits + GIE); // Enter LPM0, interrupts enabled

    }

    #pragma vector=USCIAB0TX_VECTOR
    __interrupt void USCI0TX_ISR(void)
    {
    UCA0TXBUF = string1[i++]; // TX next character

    if (i == sizeof string1 - 1) // TX over?
    IE2 &= ~UCA0TXIE; // Disable USCI_A0 TX interrupt
    }

    #pragma vector=USCIAB0RX_VECTOR
    __interrupt void USCI0RX_ISR(void)
    {
    if (UCA0RXBUF == 'u') // 'u' received?
    {
    i = 0;
    IE2 |= UCA0TXIE; // Enable USCI_A0 TX interrupt
    UCA0TXBUF = string1[i++];
    }
    }
    MSP430F2274 CC2530ZNP mini kit
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    All Replies
    • Jens-Michael Gross
      Posted by Jens-Michael Gross
      on Apr 04 2012 09:24 AM
      Guru141810 points

      Your code looks fine. And TX seems to work fine too, since if you enable TXIE manually, the hello world text gets properly transmitted.
      So my first guess would be the RX connection. Bad soldering ot something like that. Or the TX line is somehow tied to gnd/VCC, so the FTDI signal is overridden. Did you check the schematic? Is this line hardwired to the FET on your kit?

      _____________________________________
      Before posting bug reports or ask for help, do at least quick scan over this article. It applies to any kind of problem reporting. On any forum. And/or look here.
      If you cannot discuss your problem in the public, feel free to start a private conversation: click on my name and then 'start conversation'. But please do so only if you really cannot do it in a public thread, as I usually read all threads. And I prefer to answer where others can profit from it (or contribute to it) too.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • DAC CAD
      Posted by DAC CAD
      on Apr 04 2012 11:01 AM
      Prodigy60 points

      Hi Jens-Michael,

      The code works fine if I poll and remove all the interrupts. This also eliminates the connection issues that you mentioned. I do agree that I have used wires to temporarily connect the two connections along with the ground.

      At present, I am using polling in my code to overcome this issue. I still feel that there might be some software / coding issue on the MSP device. Being an evaluation kit, does TI disable features? I don't think that would be the case. 

      I prefer the interrupts but I have the code working for now. And I am using it to get over for this demo project.

      Cheers,

      DAC

      MSP 430F2274 CC2530 ZNP Minikit
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Jens-Michael Gross
      Posted by Jens-Michael Gross
      on Apr 12 2012 12:37 PM
      Guru141810 points

      I looked at your code several times over the last week (it's still on an open tab). But I don't have a clue what's wrong.
      Well, 'i' should be volatile, but it doesn't matter here (unless you want to check the current state of i in main)

      As you said, it is working when polling, so port and USCI setup and hardware are okay. And the TX ISR is working too.

      Sure, there's always the possibility of a hardware defect, but this would be a very, very unlikely one.

      I don't have any clue what's wrong with the code you posted. After all, the code isn't that complex.

      _____________________________________
      Before posting bug reports or ask for help, do at least quick scan over this article. It applies to any kind of problem reporting. On any forum. And/or look here.
      If you cannot discuss your problem in the public, feel free to start a private conversation: click on my name and then 'start conversation'. But please do so only if you really cannot do it in a public thread, as I usually read all threads. And I prefer to answer where others can profit from it (or contribute to it) too.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    TI E2E™ Community
    • Support Forums
    • Blogs
    • Videos
    • Groups
    • Site Support & Feedback
    • Settings
    TI E2E™ Community Groups
    • TI University Program
    • Make the Switch
    • Microcontroller Projects
    • Motor Drive & Control
    Other Communities
    • Deyisupport
    • Designsomething.org
    • beagleboard.org
    • TI on Element 14
    • TI on TechXchangeSM
    Other Technical & Support Resources
    • WEBENCH® Design Center
    • Product Information Centers
    • Technical Documents
    • TI Design Network
    • TI Technical Articles
    • TI Training

    All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

    Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

    Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
    TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

    TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
    embedded processors, along with software, tools and the industry’s largest sales/support staff.

    © Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy Policy | Terms of Use