• Not Answered

Checking of serial port of msp430

I am working  with msp430. If I want to check whether its serial port is working or not  and I connect its serial port to oscilloscope. What kind of waveform should I get?  A continuous square waveform or bunch of  square pulses repeating itself after a time duration.

1 Reply

  • Serial port is usually a straight high signal unless something is transmitted. During transmission you'll have at least one short low pulse (length of one bit, the start bit) and 8 data bits that may be low or high dependein on data, followed by at least on bit duration of high. The length of a bit depends on the baudrate.

    Keep in mind that RS232 signals are inverted and symmetrical. So a 'low' is 0V on the MSP/TTL signals, but 3V to 12V on RS232, while a 'high' is VCC on the MSP and -3 to -12V on RS232 (you need a transceiver such as the MAX2323 to connec the MSP to the PC COM port)

    _____________________________________

    Time to say goodbye - I don't have the time anymore to read and answer forum posts. See my bio for details.

    Before posting bug reports or ask for help, do at least quick scan over this article. It applies to any kind of problem reporting. On any forum. And/or look here.
    I'm sorry that  I can no longer provide help  in the forum or by private conversation.