• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » MSP430™ Microcontrollers » MSP430 Ultra-Low Power 16-bit Microcontroller Forum » Issue with my BSL programming
Share
MSP430™ Microcontrollers
  • Forum
  • Announcements
  • E2E Wiki
Options
  • Subscribe via RSS
MSP430 Resources
  • MSP430 Product Folder
  • MSP-EXP430G2 - MSP430 LaunchPad Value Line Development kit
  • MSP430 Getting Started Guide
  • MSP430 Microcontroller Projects
  • More Resources >
  • Forums

    Issue with my BSL programming

    This question is not answered
    chethu gowda
    Posted by chethu gowda
    on Apr 03 2012 01:37 AM
    Genius3835 points

    Hi,

    I have written a BSL for MSP4305529 which is used to program the main application of the MCU over UART.  In BSL I am not making use of any interrupt vectors and everything is done using the polling mechanism.

    Here I am not making use of the BSL memory in the flash as I need to implement this system on MSP430G2403 (which does not have the BSL memory). So My BSL sits at the location 0xF800 .

    I am sending the TI-txt file's bytes through UART and receiving the same on the MCU's BSL and writing the same on the flash's memory that I have allocated for the main application i.e 0x4400-0xF7FF (This I am configuring through the linker file lnk430f5529.xcl). I am writing the interrupt vectors of the main application in the corresponding locations except the reset vector (It always remains the BSL's).

    On boot up I am handing over the control from the BSL to main applicatoin using  a simple branch operation,

    i.e asm("br #0x4400");

    But the main application is not working as expected. If I take the memory dump after programming I can see the data in the flash is exactly same as that of TI-txt file.

    what could be the problem with this. (For smaller programs like UART checking program and flashing LED program its working fine)

    Thanks & Regards,

    cbn

    BSL
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    All Replies
    • old_cow_yellow
      Posted by old_cow_yellow
      on Apr 03 2012 02:46 AM
      Guru26585 points

      I assume you are using F5529, not G2403. Are you?

      A few possible causes:

      a. The contains of 0x4400-0xF7FF are not exactly the same as the TI-txt file. Some bits are not the same and you did not notice that.

      b. The Flash is not erased completely or written completely. The can be read, but cannot execute reliably.

      c. The code is not correct to begin with and dose not work as you expected.

      d. The code assumes that the registers just come out of reset and thus have the BOR values. But your BSL has changed them already.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • chethu gowda
      Posted by chethu gowda
      on Apr 03 2012 08:59 AM
      Genius3835 points

      There was a small oversighted mistake,

      My window side program was not made compatible with the larger TI-txt files which have intermittent gaps which need to be skipped or filled with 0xFF.

      Now its working fine.

      Thanks & Regards,

      cbn

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Katie Enderle
      Posted by Katie Enderle
      on Apr 03 2012 10:40 AM
      Genius13395 points

      Hi,

      I realize there may be a reason for you to want to implement a custom BSL, but I wanted to point out in case you were not aware that the MSP430G2403 is actually one of the value line parts that does already include a BSL in ROM (all G2xx3 parts have this, G2xx1 and G2xx2 do not). There are still reasons you might want to have a custom BSL though, if you wanted to use a different communications interface for example.

      Regards,

      Katie

      Please click the Verify Answer button on this post if it answers your question.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Bhaumik Shah
      Posted by Bhaumik Shah
      on Apr 03 2012 10:58 AM
      Prodigy150 points

      Hi every one,

      I am new to BSL programming. I have couple of quarries to get started.

      1) Do we need to flash MSP430 Device with BSL 1st  ?

      2) Is BSL different for device variants of MSP430 ?

      Please help.

      Regard s

      Bhaumik Shah

      BSL BSL430
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Katie Enderle
      Posted by Katie Enderle
      on Apr 03 2012 11:02 AM
      Genius13395 points

      Hi Bhaumik,

      You can find the answers to these questions in the MSP430 Programming Via the BSL User's Guide (SLAU319). and on this wiki page: http://processors.wiki.ti.com/index.php/BSL_(MSP430)

      Regards,

      Katie

      Please click the Verify Answer button on this post if it answers your question.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • chethu gowda
      Posted by chethu gowda
      on Apr 03 2012 22:19 PM
      Genius3835 points

      Hi Katie Enderle,

      Katie Enderle

      There are still reasons you might want to have a custom BSL though, if you wanted to use a different communications interface for example

      The only reason to implement the custom BSL is that , the custom BSL has the full control over the main application about it's location in flash, it's execution, etc.

      I am using my own simple communication protocol built over UART for flashing the main application.

      Please let me know if anything is mistaken in this.

      In addition to flashing main application via BSL, only through BSL the application shall be launched always (as only the BSL knows the main application location).

      My intention is to blow the fuse once my BSL is loaded into the controller and there by allowing programming the controller only through my BSL.

      Please let me know if there anything flaw in this.

      Thanks & Regards,

      cbn

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • old_cow_yellow
      Posted by old_cow_yellow
      on Apr 03 2012 23:05 PM
      Guru26585 points

      I have three questions:

      1. G2303 has only 4KB of Flash. How big is your BSL code?

      2. How is your BSL protected from being altered (unintentionally) by your main program?

      3. How is your BSL entered? If for some reason, your main program crashed, can one still start your BSL? (TI BSL has a hardware sequence to start BSL. Can it start your BSL?)


      I am trying to implement BSL for G2xx1 and G2xx2. I am stuck with no good answers for the above 3 questions.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • chethu gowda
      Posted by chethu gowda
      on Apr 03 2012 23:52 PM
      Genius3835 points

      Hi old_cow_yellow,

      old_cow_yellow

      1. G2303 has only 4KB of Flash. How big is your BSL code?

      My BSL is ~1100 Bytes so keeping 3 blocks of main flash memory, i.e 1536 Bytes for the BSL, remaining 2560 Bytes can be used for the main application.

      (Here My main application is expected to be smaller one) Also the main intention behind this BSL is to provide controlled access to execute the main application.

      Since I am blowing the fuse once I flash the BSL, I am providing the programming facility over UART through BSL so that the third party can program it's main application.

      Depending on the main applicatoin size, I can opt for G2403 which has 8kB of main memory.


      old_cow_yellow

      2. How is your BSL protected from being altered (unintentionally) by your main program?

      Currently a severe care is taken in the main application design to not to disturb the BSL.(I have not yet found the way to protect that particular part of the flash where BSL resides) Please let me know if you find any mechanism for the same.


       

      old_cow_yellow

      3. How is your BSL entered? If for some reason, your main program crashed, can one still start your BSL? (TI BSL has a hardware sequence to start BSL. Can it start your BSL?)

      The reset vector contains the BSL's address, so unconditionally The BSL is invoked on reset. As I mentioned in my earlier threads, my BSL is just another application(App1) which on request will handover the control to the main application(App2).


      Please let me know if anything is wrong in my explaination.

      Thanks & Regards,

      cbn

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • old_cow_yellow
      Posted by old_cow_yellow
      on Apr 04 2012 16:16 PM
      Guru26585 points

      Chethu,

      Using a scheme very similar to yours, I developed sort of a "customized BSL" for the MSP-EXP430FR5739 experimental board.

      Like yours, the real Reset Vector (at 0xFFFE) always points to the beginning of my BLS. I implemented a “virtual Reset Vector” inside my BSL. After any kind of reset, my BSL will take charge. It looks at the cause of the reset and decides whether to execute Application according to the “virtual Reset Vector”.
       
      FR57xx has Memory Protection Unit. I use that to protect my BSL as well as all the Interrupt Vectors. (total 512 Bytes from 0xFE00 to 0xFFFF.)  When the TI-txt tells my BSL to load the Reset Vector, my BSL will actually put that in the “virtual Reset Vector”. Also, if the Application program crashes and cause a reset, my BSL will trap unexpected resets too.

      This works fine for FR5739, but I could not easily port it to G2xx. (Especially for the low-end chips.) I now have some idea, but un-tried yet. I think I can squeeze an abridged BSL into Info-Flash-B, -C, and –D. This is at the cost of a special PC program. Unlike the one for FR57xx, which only needs a Terminal Emulator at the PC side to send TI-txt file, this one needs the PC to send binary code with a special handshaking “protocol”.

      Both the MSP-EXP430FR5739 board and the LaunchPad board has (a) built-in USB to Virtual COM Port, (b) Reset button, and (c) firmware readable button. I use (b) and (c) together to start BSL in loader mode. I use (a) to do the actual loading.

      Regards,

      OCY

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • TonyKao
      Posted by TonyKao
      on Apr 04 2012 16:51 PM
      Genius3770 points

      Hi chethu,

      Could I suggest a simpler "gate-keeper" bootloader where it normally loads the main program but can load the ROM BSL under certain controlled conditions (i.e. not just the normal BSL sequences on RST/TEST)?

      Or you can just use the ROM BSL as-is.

      The ROM BSL already has the capacity to be accessed through UART and be password protected, where if you enter the wrong password it automatically enters mass-erase mode thus ensuring the security of your code.

      Tony

      Edited: FYI, you can still access the ROM BSL after you've blown the JTAG fuse.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • chethu gowda
      Posted by chethu gowda
      on Apr 05 2012 00:54 AM
      Genius3835 points

      Hi old_cow_yellow,

      old_cow_yellow
      FR57xx has Memory Protection Unit

      The FR57xx has the segment wise protection facility which is sufficient to protect the BSL. But no such features available in G2xx which is the reason for problem with BSL protection.

      In addition, I have a doubt, I think I had pointed it in one of my previous posts,

      FR5739 has a BSL memory in ROM which is specified in the memory organization section of the data sheet  also the functional block diagram shows the boot ROM. But why its not the same in case of G2304, the ROM BSL is not shown anywhere.

      is it possible to program the G2xx after blowing the JTAG fuse, via the ROM BSL through UART like it can be done for FRxx and F55xx,

      old_cow_yellow
      squeeze an abridged BSL into Info-Flash-B, -C, and –D. This is at the cost of a special PC program

      This was my original idea, but the main constraint was very less information memory in G2xx.

       

      Thanks & Regards,

      cbn

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • chethu gowda
      Posted by chethu gowda
      on Apr 05 2012 00:59 AM
      Genius3835 points

      Hi Katie Enderle,

      Sorry I missed out a point in my previous post,

      Katie Enderle
      but I wanted to point out in case you were not aware that the MSP430G2403 is actually one of the value line parts that does already include a BSL in ROM (all G2xx3 parts have this, G2xx1 and G2xx2 do not).

      Nowhere in the data sheet of G2xx (SLAS734D–APRIL 2011–REVISED NOVEMBER 2011) its mentioned about the BSL ROM.

      Please let  me know if I have to refer any other documents which says about the G2xx3  parts having the BSL ROM.

      Thanks & Regards,

      cbn

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • old_cow_yellow
      Posted by old_cow_yellow
      on Apr 05 2012 02:39 AM
      Guru26585 points

      Chethu,

      G2xx1 and G2xx2 chips do not have ROM BSL.

      G2xx3 and FR57xx chips do have ROM BSL. But to use it, you need extra hardware so that the PC can initiate BSL Entry Sequence and can use parity bit.  The LaunchPad and FR5739 Exp Board hardware do not support these features.

      The BSL code on the MSP430 side can be squeezed to ~192 Bytes and put in the Info-Flash.

      OCY

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • chethu gowda
      Posted by chethu gowda
      on Apr 05 2012 04:40 AM
      Genius3835 points

      Hi old_cow_yellow,

      old_cow_yellow
      G2xx3 and FR57xx chips do have ROM BSL.

      My main intention in providing the programming feature through custom BSL is to secure some very important and sensitive data which is stored as part of the BSL  or in some secured location (My understanding was if I blow the JTAG fuse the flash content will be secure and to support my point the datasheet  (SLAS734D–APRIL 2011–REVISED NOVEMBER 2011) does not say anything about the ROM BSL of the G2xx3 using which the flash can be read/written).

      But as you are saying the G2xx has the ROM BSL, can someone read the flash content through this ROM BSL?

      If its possible to read the flash content through ROM BSL, how to protect this sensitive data from reading by someone?

       

      Thanks & Regards,

      cbn

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • chethu gowda
      Posted by chethu gowda
      on Apr 05 2012 05:04 AM
      Genius3835 points

      Hi old_cow_yellow & everyone,

      chethu gowda
      My understanding was if I blow the JTAG fuse the flash content will be secure and to support my point the datasheet  (SLAS734D–APRIL 2011–REVISED NOVEMBER 2011) does not say anything about the ROM BSL

      I sincerely apologize for the above statement which is completely wrong. Actually in the G2xx3's datasheet (SLAS734D) there is a clear mentioning about the BSL.

      chethu gowda

      If its possible to read the flash content through ROM BSL, how to protect this sensitive data from reading by someone?

      The flash read/write operation through ROM BSL can be completely disabled by disabling the BSL using the BSLSKEY. Writing the word 0xAA55 at this location will completely disable the BSL. So I still retain the security for my data stored in the flash :)

      I hope there is no other ways through which the flash data can be read/overwritten after blowing the JTAG fuse & disabling the BSL, if you think its still possible pls let me know.

      Thanks & Regards,

      cbn

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    12
    TI E2E™ Community
    • Support Forums
    • Blogs
    • Videos
    • Groups
    • Site Support & Feedback
    • Settings
    TI E2E™ Community Groups
    • TI University Program
    • Make the Switch
    • Microcontroller Projects
    • Motor Drive & Control
    Other Communities
    • Deyisupport
    • Designsomething.org
    • beagleboard.org
    • TI on Element 14
    • TI on TechXchangeSM
    Other Technical & Support Resources
    • WEBENCH® Design Center
    • Product Information Centers
    • Technical Documents
    • TI Design Network
    • TI Technical Articles
    • TI Training

    All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

    Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

    Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
    TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

    TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
    embedded processors, along with software, tools and the industry’s largest sales/support staff.

    © Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy Policy | Terms of Use