• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » MSP430™ Microcontrollers » MSP430 Ultra-Low Power 16-bit Microcontroller Forum » Need help in USI SPI COMMUNICATION between two launchpads(MSP430G2231)
Share
MSP430™ Microcontrollers
  • Forum
  • Announcements
  • E2E Wiki
Options
  • Subscribe via RSS
MSP430 Resources
  • MSP430 Product Folder
  • MSP-EXP430G2 - MSP430 LaunchPad Value Line Development kit
  • MSP430 Getting Started Guide
  • MSP430 Microcontroller Projects
  • More Resources >
  • Forums

    Need help in USI SPI COMMUNICATION between two launchpads(MSP430G2231)

    This question is not answered
    sudeep nandiki
    Posted by sudeep nandiki
    on Apr 03 2012 18:05 PM
    Prodigy100 points

    Hii

    i am very new to MSP430G2231 and i am trying to establish spi link between two launchpads to transfer some data. by assigning the required DATA to USISRL register  will transmit the data from one launchpad to other or any PINs have to be used. please help me in this.

    thank you

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    All Replies
    • Jens-Michael Gross
      Posted by Jens-Michael Gross
      on Apr 04 2012 12:02 PM
      Guru139970 points

      sudeep nandiki
      by assigning the required DATA to USISRL register  will transmit the data from one launchpad to other or any PINs have to be used

      Well, there is no wireless communication between LaunchPads. So yes. pins need to be used.

      Depending on the processor you have on the LaunchPad, different pins are used and in a different way. Some G2 processors have an USI module, some an USCI, and the two are completely different to handle.

      However, an PSI communication needs an absolute minimum of 4 wires between the two peers: SOMI, SIMO, SCLK and GND. You may also add VCC if you want to power both from one supply, and a snychronisation signal that is controlled/checked by GPIO. Almost every commercial SPI slave requires such a signal, usually called chip select (CS).
      And maybe an interrupt signal that tells teh SPI master that the SPi slave has something to tell.

      _____________________________________
      Before posting bug reports or ask for help, do at least quick scan over this article. It applies to any kind of problem reporting. On any forum. And/or look here.
      If you cannot discuss your problem in the public, feel free to start a private conversation: click on my name and then 'start conversation'. But please do so only if you really cannot do it in a public thread, as I usually read all threads. And I prefer to answer where others can profit from it (or contribute to it) too.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • sudeep nandiki
      Posted by sudeep nandiki
      on Apr 05 2012 07:50 AM
      Prodigy100 points

      Hi Jens-Michael Gross

             thank you very much , i used slave only in receiving mode and master only in transmitting mode. can you please check the code pasted below. please

      master


      #include <msp430g2231.h>
      void main(void)
      {
        volatile unsigned int i;

        WDTCTL = WDTPW + WDTHOLD;             // Stop watchdog timer
        P1OUT =  0x10;                        // P1.4 set, else reset
        P1REN |= 0x10;                        // P1.4 pullup
        P1SEL |=0x06;
        //P1DIR = 0x01;                         // P1.0 output, else input
        USICTL0 |= USIPE7 +  USIPE6 + USIPE5 + USIMST + USIOE; // Port, SPI master
        USICTL1 |= USIIE;                     // Counter interrupt, flag remains set
        USICKCTL = USIDIV_4 + USISSEL_2;      // /16 SMCLK
        USICTL0 &= ~USISWRST;                 // USI released for operation
        USISRL = 0X02;                        // init-load data

        P1DIR |= 0x04;                        // Reset Slave
        P1DIR &= ~0x04;
        for (i = 0xFFF; i > 0; i--);          // Time for slave to ready
        USICNT = 8;                           // init-load counter

      while (1)                                 // Loop
      {
        unsigned i;
        for (i = 0xFFFF; i > 0; i--);           // Delay
        while (!(USIIFG & USICTL1));            // Counter clear?
        USISRL=0X02;

                         // Read data are ready to be written
        USICNT = 8;         // re-load counter
        for (i = 0xFFFF; i > 0; i--);

        USISRL=0X03;

        USICNT=8;
      }
      }

      slave

      #include <msp430g2231.h>


      void main(void)
      {
        WDTCTL = WDTPW + WDTHOLD;             // Stop watchdog timer
       // P1OUT =  0x10;                        // P1.4 set, else reset
       // P1REN |= 0x10;                        // P1.4 pullup
        //P1DIR = 0x01;                       // P1.0 output, else input
         // P1SEL |=0x0A;
        USICTL0 |= USIPE7  + USIPE5 + USIOE; // Port, SPI slave
        USICTL1 |= USIIE;                     // Counter interrupt, flag remains set
        USICTL0 &= ~USISWRST;                 // USI released for operation
        //USISRL = P1IN;                        // init-load data
        USICNT = 8;                           // init-load counter
        while (1)                                 // Loop
         {

            unsigned i,m;
           for (i = 0xFFFF; i > 0; i--);           // Delay
           while (!(USIIFG & USICTL1));            // Counter clear?
          m=USISRL;
           if( m== 0X02)
               P1OUT |=0x01;
               else
                   P1OUT &=~0x01;
                  USICNT = 8;                             // re-load counter
         }
      }



      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    TI E2E™ Community
    • Support Forums
    • Blogs
    • Videos
    • Groups
    • Site Support & Feedback
    • Settings
    TI E2E™ Community Groups
    • TI University Program
    • Make the Switch
    • Microcontroller Projects
    • Motor Drive & Control
    Other Communities
    • Deyisupport
    • Designsomething.org
    • beagleboard.org
    • TI on Element 14
    • TI on TechXchangeSM
    Other Technical & Support Resources
    • WEBENCH® Design Center
    • Product Information Centers
    • Technical Documents
    • TI Design Network
    • TI Technical Articles
    • TI Training

    All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

    Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

    Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
    TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

    TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
    embedded processors, along with software, tools and the industry’s largest sales/support staff.

    © Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy Policy | Terms of Use