• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » MSP430™ Microcontrollers » MSP430 Ultra-Low Power 16-bit Microcontroller Forum » hexadecimal to ASCII
Share
MSP430™ Microcontrollers
  • Forum
  • Announcements
  • E2E Wiki
Options
  • Subscribe via RSS
MSP430 Resources
  • MSP430 Product Folder
  • MSP-EXP430G2 - MSP430 LaunchPad Value Line Development kit
  • MSP430 Getting Started Guide
  • MSP430 Microcontroller Projects
  • More Resources >
  • Forums

    hexadecimal to ASCII

    This question is not answered
    Preston Lortie
    Posted by Preston Lortie
    on Apr 06 2012 17:38 PM
    Prodigy80 points

    I am doing an ADC12 conversion and sending this value to ADC12MEM0. Once the ADC12 is complete, I am sending the ADC12MEM0 values upper and lower 8 bits to the hyperterminal.  I understand that it is simply sending the hex values in the register over as ascii, but I would like to display these values as hex on the hyperterminal. I would like to copy the register exactly as it appears to the hyperterminal (0x0FFF on ADC12MEM0 would make hyperterminal display 0x0FFF... etc.). I have looked at hex to ascii tables and I understand how this works, but I have no idea how to write this as code in code composer studio. Is there some advice you could give me or an example code I can look at to better understand. Below I have provided my code. Thanks!

    # include <msp430xG46x.h>

    volatile unsigned int temp;
    volatile unsigned int i;


    void main(void)
    {
    WDTCTL = WDTPW+WDTHOLD; // Stop watchdog
    // Initialization of ADC12//

    P6SEL |= 0x01; // Enable A/D channel A0
    ADC12CTL0 &= ~ENC;
    ADC12CTL0 = ADC12ON + SHT0_2 + REFON + REF2_5V+MSC; // turn on ADC12, set samp time
    ADC12CTL1 = SHP+CONSEQ_2; // Use sampling timer
    ADC12MCTL0 = SREF_1 + INCH_0; // Vr+=VeREF+ (external)
    ADC12CTL0 |= ENC; // Enable conversions
    // Initialization of Rs-232//
    FLL_CTL0 |= XCAP14PF; // Configure load caps

    do
    {
    IFG1 &= ~OFIFG; // Clear OSCFault flag
    //_delay_cycles(50000); // Time for flag to set
    }
    while ((IFG1 & OFIFG)); // OSCFault flag still set?
    P2SEL |= 0x30; // P2.4,5 = USCI_A0 RXD/TXD

    UCA0CTL1 |= UCSSEL_1; // CLK = ACLK
    UCA0BR0 = 0x03; // 32k/9600 - 13.65
    UCA0BR1 = 0x00; //
    UCA0MCTL = 0x06; // Modulation
    UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
    IE2 |= UCA0TXIE + UCA0RXIE; // enable RXD and TXD interrupt;
    while (1)
    {
    // ADC loop //
    ADC12CTL0 |= ADC12SC; // Start conversions
    //while (!(ADC12IFG & 0x0001)); // Conversion done?
    temp = ADC12MEM0; // Move result
    __no_operation(); // SET BREAKPOINT HERE
    // RS-232 loop //
    UCA0TXBUF = temp; // send lower part
    __no_operation();
    //while(!(IFG2 & UCA0TXIFG))
    //{
    //_delay_cycles(1000); // wait for first transmit
    //}
    UCA0TXBUF = temp >> 8;// send upper part
    __no_operation();
    // _delay_cycles(1000);
    //UCA0TXBUF = temp;
    }
    }

    ADC12 ascii hexadecimal
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    All Replies
    • Andy Neil
      Posted by Andy Neil
      on Apr 08 2012 01:35 AM
      Guru31775 points

      Have you given up trying to do this "manually", then?

      Preston Lortie
      it would not print serially to PUTTY

      So you've switched from Hyperterminal - are you sure that you have PUTTY correctly configured?

      Preston Lortie
      do I have to do anything special to get the printf command to work?

      Note that printf() is a library function - not a "command".

      The thing with printf() is - where does the output go?
      The standard 'C' library defines it to go to stdout; on a PC, that is "the console"  - but what does that mean on a microcontroller?

      You need to check your CCS documentation to see whether there is a default, and/or whether you have to provide some "driver" for it...

      Alternatively, you could just use sprintf() to put the output into a buffer, and then send that buffer "manually"...

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Andy Neil
      Posted by Andy Neil
      on Apr 08 2012 01:42 AM
      Guru31775 points

      This Wiki page contains a link to the MSP430 Compiler Manual:

      http://processors.wiki.ti.com/index.php/Printf_support_in_compiler

       

      MSP430 Compiler Manual
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Roberto Romano
      Posted by Roberto Romano
      on Apr 08 2012 05:16 AM
      Mastermind6840 points

      Preston Lortie
      IE2 |= UCA0TXIE + UCA0RXIE; // enable RXD and TXD interrupt;

       Hi Preston, first don't enable interrupt if no service routine are in place, this can generate program restart you cannot explain why.

      Preston Lortie
      UCA0TXBUF = temp; // send lower part
      __no_operation();
      //while(!(IFG2 & UCA0TXIFG))
      //{
      //_delay_cycles(1000); // wait for first transmit
      //}
      UCA0TXBUF = temp >> 8;// send upper part
      __no_operation();
      // _delay_cycles(1000);
      //UCA0TXBUF = temp;

       Don't try this way build some libraries instead:

      void Putch(unsigned char ch)
      {
          while (!(IFG2&UCA0TXIFG))           // USCI_A0 TX buffer ready?
            __no_operation();
          UCA0TXBUF = ch;                     // TX -> character
      }

      void PutStr (const char * ch)
      {
         while (*ch)
            Putch(*ch++);
      }

      after that use sprintf and pass the buffer string to PutStr

      The putch routine is the basic of printf usage but use a smarter way writing some code to output:

      char mybuffer[40];

      sprintf(mybuffer,"hello world 0x%x\n",temp);

      PutStr(mybuffer);

       Regards

       Roberto


       Please login & click    Verify Answer    if this post answered your question.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Jens-Michael Gross
      Posted by Jens-Michael Gross
      on Apr 11 2012 06:16 AM
      Guru139900 points

      While printf is convenient, it is also slow, requires lots of stack space and significantly raises the size of the binary.

      Speed is an issue if you try to send the result form within an ISR. Don't do this. You'll run into timing problems rather sooner than later.
      Stack usage is an issue on MSPs with low ram. Like the G series. Or the 1232.
      High size is a problem not only on MSPs with small flash, but even on bigger ones, it can make the generated binary larger than the allowed size for the free compiler versions. And paying several hundred bucks for a full compiler license jsut to use printf...

      However, a fast and cheap version can be implemented easily (and there is some code already posted in an older thread):

      Count, how often you can subtract 10.000 from the value before it becoems <10000. Do NOT use "/" as divisions are slooow (this also applies to "%"). Do really a loop
      for (count='0'; value>10000; count++, value-=10000);

      The '0' is not a typo! After the loop, count will directly hold the ASCII letter representing the 10k's and can be directly sent to HyperTerm.

      Then repeat for 1000, 100, 10. Finally, add '0' to the remaining value for the last digit. You'll get a 5 digit decimal number with leading zeroes. Fast and small and no stack usage.
      You can turn it into a function by passing the 'digit' value. A bit slower then, requires a bit stack, but even smaller code :) And can be used for ASCII conversions of octals or even binary numbers too :)

      _____________________________________
      Before posting bug reports or ask for help, do at least quick scan over this article. It applies to any kind of problem reporting. On any forum. And/or look here.
      If you cannot discuss your problem in the public, feel free to start a private conversation: click on my name and then 'start conversation'. But please do so only if you really cannot do it in a public thread, as I usually read all threads. And I prefer to answer where others can profit from it (or contribute to it) too.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Bruce Mitchell
      Posted by Bruce Mitchell
      on May 08 2012 12:44 PM
      Intellectual255 points

      How about this

       

      static const char hex_string[] = "0123456789ABCDEF";


      void

      print_hex(uint8_t c)
      {
      char output_short[] = {"XX"};

      output_short[
      0] = hex_string[(c >> 4) & 0x0F];
      output_short[
      1] = hex_string[ c & 0x0F];

      TXString(output_short,
      2 /* sizeof(output_short) */ );
      }

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Roberto Romano
      Posted by Roberto Romano
      on May 08 2012 15:46 PM
      Mastermind6840 points

      Bruce Mitchell
      print_hex(uint8_t c)
      {
      char output_short[] = {"XX"};

       Hi this part generate string on stack so time and space are wasted out...

       May be better to direct transfer character calling two time the txstring:

      print_hex(uint8_t c)
      {
      TXString(hex_string[(c >> 4) & 0x0F],1);
      TXString(hex_string[ c & 0x0F],1);
      }

      //Also consider to convert bin to HEX by function:

      char bin2hexdigit(char c)

      {

      c&=0x0f; // 4 bit

       if(c>9) c+=('A'-'0'-10);   // ASCII offset from number to capital letters

      // if(c>9) c+=('a'-'0'-10);   // ASCII offset from number to small letters

      return(c+'0');  // Add character offset to binary value

      }

       The value ('A'-'0'-10) evaluate to 7 and is the  difference to add to character '0' to obtain the character 'A' when binary value is 10, compiler calculate this value but I used this form for clarity.

       also the difference between small and capital is 32 so to convert to hex with small letter need add 39 -> ('a'-'0'-10) instead of 7

       Regards

       Roberto


       Please login & click    Verify Answer    if this post answered your question.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Bard Ciou
      Posted by Bard Ciou
      on Apr 29 2013 21:44 PM
      Prodigy180 points

      Hi Roberto

      I think use sprintf will increase more memory size

      You can try use a sub-function like this...

      //in while loop

      TX_Byte((uint8_t)uartBuffer[0]); //Byte0, Carriage return
      uartBuffer[0] = 0x0D;

      //HexToASCII

      void TX_Byte (uint8_t TX_DATA)
      {
      while (!(IFG2&UCA0TXIFG)); // USCI_A0 TX buffer ready?
      UCA0TXBUF = (unsigned char *)TX_DATA; // TX_DATA
      }

      Best Regards,

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    12
    TI E2E™ Community
    • Support Forums
    • Blogs
    • Videos
    • Groups
    • Site Support & Feedback
    • Settings
    TI E2E™ Community Groups
    • TI University Program
    • Make the Switch
    • Microcontroller Projects
    • Motor Drive & Control
    Other Communities
    • Deyisupport
    • Designsomething.org
    • beagleboard.org
    • TI on Element 14
    • TI on TechXchangeSM
    Other Technical & Support Resources
    • WEBENCH® Design Center
    • Product Information Centers
    • Technical Documents
    • TI Design Network
    • TI Technical Articles
    • TI Training

    All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

    Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

    Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
    TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

    TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
    embedded processors, along with software, tools and the industry’s largest sales/support staff.

    © Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy Policy | Terms of Use