• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » MSP430™ Microcontrollers » MSP430 Ultra-Low Power 16-bit Microcontroller Forum » Launchpad Based MSP430 UART BSL interface (slaa535)
Share
MSP430™ Microcontrollers
  • Forum
  • Announcements
  • E2E Wiki
Options
  • Subscribe via RSS
MSP430 Resources
  • MSP430 Product Folder
  • MSP-EXP430G2 - MSP430 LaunchPad Value Line Development kit
  • MSP430 Getting Started Guide
  • MSP430 Microcontroller Projects
  • More Resources >
  • Forums

    Launchpad Based MSP430 UART BSL interface (slaa535)

    This question is answered
    old_cow_yellow
    Posted by old_cow_yellow
    on May 29 2012 17:53 PM
    Guru25715 points

    Has anybody tried the scheme described in TI Application Note Launchpad-Based MSP430 UART BSL Interface? See slaa535.pdf and slaa535.zip or:

    http://focus.ti.com/mcu/docs/litabsmultiplefilelist.tsp?sectionId=96&tabId=1502&literatureNumber=slaa535&docCategoryId=1&familyId=342

    I have some serious doubt about this scheme.

    Launchpad has an on-board emulator with USB interface that supports an Application UART (Virtual COM PORT) to communicate with the PC. The said Application Note tries to use this VCP as the interface to do BSL for another target such as the MSP430F5438A. But as far as I know, the LaunchPad Application UART does not support parity and the MSP430F5438A BSL requires even parity. So, how is that going to work?

    slaa535
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    All Replies
    • Leo Hendrawan
      Posted by Leo Hendrawan
      on May 30 2012 02:54 AM
      Suggested Answer
      Mastermind27025 points

      Hi OCY,

      nice catch there. I wrote the app note, and tested it on the F5438A which has Timer_A UART, and it should work. I also just realized that the Launchpad UART does not support the parity bit as required by the BSL specs. I have been also struggling to make it work on the CC430 which has the hardware USCI UART, and after a quick investigation, here are my first suggestion:

      - the app note will only work with 5xx/6xx devices which have Timer_A UART (e.g. the F5438A). The reason of this is because in the BSL PI module using the Timer_A UART, the UART frame will not be rejected if the parity is not correct (or even does not exist). Take a look at the receiveByte() function in BSL430_PI_TA.c (you can download this on SLAA450 App note):

      char receiveByte()
      {
        int bitCount = 9; // Load Bit counter
        int dataByte = 0; 
        TZNCCTL_RX = SCS + OUTMOD0 + CM1 + CAP; // Sync, Neg Edge, Cap
        while( !(TZNCCTL_RX & CCIFG) ); // wait for first char
        TZNCCTL_RX &= ~ (CAP+CCIFG); // Switch from capture to compare mode, turn off interrupt
        TZNCCR_RX += BitTime_5;
        while( bitCount > 0 )
        {
          TZNCCR_RX += BitTime;
          TZNCCTL_RX &= ~CCIFG;
          while( !(TZNCCTL_RX & CCIFG) ); // time out one char
          dataByte = dataByte >> 1;
          if (TZNCCTL_RX & SCCI) // Get bit waiting in receive latch
          {
            dataByte |= 0x100;
          }
          bitCount --;
        }
        return (dataByte&0xFF);
      }

      As you can see above, no matter what happen, the function will always return the received byte without really checking the parity.

      - This is of course different for the hardware USCI UART BSL like the one in CC430 devices. The reason is that the frame will be rejected by the USCI hardware if the parity is not correct or does not exist:

      char receiveByte()
      {
        while( !(UCA0IFG & UCRXIFG)); // wait for RX flag
        return UCA0RXBUF;
      }

      As can be seen above, the receiveByte() function in this case just waits until the UCRXIFG set by the hardware. This of course will not happen as long as the parity is not the correct one.

      This is basically my pre-assumption, and i will try to investigate further. However as mentioned, it should work with the F543xA devices with the Timer_A UART BSL.

      UPDATE: i have talked to the tools team, and they confirmed that this is the reason why the app note works on the device with Timer_A based UART BSL but not on the hardware UART BSL. 

      Hope this helps.

      Regards,

      Leo Hendrawan


      - Now that my signature has caught your attention, please click the "Verify Answer" button if this post answers your question. Thanks! -

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Leo Hendrawan
      Posted by Leo Hendrawan
      on May 30 2012 09:45 AM
      Mastermind27025 points

      just to add some information. The basic idea of this application note is to provide a low-cost solution for the gap of UART BSL hardware interface which we haven't had since sometime. So i came to the idea by thinking what is the most known MSP430 hardware tools with UART interface, which is of course Launchpad (unfortunatelly i missed the point with the parity bit, ouch..).

      At first, i thought about implementing the solution by store and forward solution instead of bit-banging the GPIO to bridge the UART data, however because currently all G2xx devices have only maximum 1 serial interface, i needed to implement another Timer_A based UART interface. After some tests, i found that the Launchpad somehow could not cope with the speed (even with 9600 baud) by using this kind of solution.  This will work if i would add some delay in sending every byte in the BSL Scripter code, however after discussing with the MSP430 tools team, they want to implement something which could work with the current available  BSL_Scripter solution without any modification, and therefore i saw only the only possibility is to use the bit banging mechanism.

      I just tested another solution by using the MSP430G2553 with store and forward mechanism (with some delay addition in the BSL Scripter code) and it works also for the CC430 hardware UART BSL. The idea is to use Timer_A interface between PC and Launchpad (both working with 9600 baud and no parity), and USCI interface between Launchpad and MSP430 target (with 9600 baud, even parity). This should also work, but the BSL Scripter can not be used "as is" without any modification.

      I am trying to discuss with the tools team whether it is possible to add the UART feature of 9600 baud with even parity into the Launchpad emulator firmware. However, this is of course not a short term solution. For short term solution, i would advise to use the G2553 which has USCI interface and use the modified BSL Scripter.

      Hope everything is clear now.

      Regards,

      Leo Hendrawan


      - Now that my signature has caught your attention, please click the "Verify Answer" button if this post answers your question. Thanks! -

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • old_cow_yellow
      Posted by old_cow_yellow
      on May 30 2012 12:10 PM
      Guru25715 points

      Leo,

      Thank you for the explanation. I have a few questions:

      About the current BSL Scriptor in COM Port mode (as oppose to USB mode):

      (a) After it wiggles RST and TEST/TCLK, it sends SYNC and waits for ACK. How long does it wait? If there is no ACK, I think it sends SYNC and waits for ACK again. How often does it re-try? For how many times before it gives up?

      (b) When the Scriptor sends a command, I think there is a gap between the bytes. Is this true? Is there about 1 msec between the Stop-Bit and the next Start-Bit?

      (c) With the exception of handling MSP430F54xx (none-A version), I think Scriptor always send bytes with even-parity. Is this true? Does it check parity of incoming bytes from MSP430? Are parity error ignored?

      About the BSL code inside MSP430 or CC430 chips that use COM Port (not USB or RF):

      (d) I think the BSL code can choose to check or ignore parity bit. This is independent of whether they use Timer-UART or hardware-UART. For example,I know most F1xx and F2xx BSL use Timer-UART and they do check parity. You cited two actual BSL code, one ignores parity, the other one rejects bytes with parity-error.  What about other F5xx and F6xx?

      (e) What about FRAM chips and Wolverine?

      I do not have a need of a BSL interface for myself. I asked these questions just out of curiosity.

      Regards,

      OCY

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Leo Hendrawan
      Posted by Leo Hendrawan
      on May 30 2012 15:49 PM
      Verified Answer
      Verified by old_cow_yellow
      Mastermind27025 points

      Hi OCY,

      old_cow_yellow

      (a) After it wiggles RST and TEST/TCLK, it sends SYNC and waits for ACK. How long does it wait? If there is no ACK, I think it sends SYNC and waits for ACK again. How often does it re-try? For how many times before it gives up?

      I think you have mistaken between the Flash based BSL (on 5xx/6xx devices, works with BSL Scripter) and the ROM based BSL (older 1xx/2xx/4xx devices, work with deprecated BSL DEMO). The protocol is completely different between the two BSL types, and each of them is described in SLAU319 chapter 2 and 3. In this case, i think you are talking about the ROM based BSL, and the software tools for this is the BSL DEMO (please refer to this wiki page: http://processors.wiki.ti.com/index.php/BSL_(MSP430)#BSL_Tools). I am not really familiar with the BSL DEMO software, but the source code should be available also in the SLAU319 associated file.

      old_cow_yellow

      (b) When the Scriptor sends a command, I think there is a gap between the bytes. Is this true? Is there about 1 msec between the Stop-Bit and the next Start-Bit?

      Well, i am not an expert in Windows programming, but according to the BSL Scripter sources (which you can also download with the associated files of SLAU319), the writeByte() function does not contain any delay mechanism (i added delay however in the case of using my custom launchpad based solution with G2553). The transmission of series of bytes should be quite fast, i believe. Regarding the 1 ms delay, i am not sure about this since i have never measured this myself. If you want to know how the BSL Scripter works, i would suggest to download Microsoft Visual Studio C++ 2010 express edition (it's free), and then open the project file which i created a while ago here:

      http://processors.wiki.ti.com/images/b/b0/BSL_Scripter_VC%2B%2B.zip

      old_cow_yellow

      (c) With the exception of handling MSP430F54xx (none-A version), I think Scriptor always send bytes with even-parity. Is this true? Does it check parity of incoming bytes from MSP430? Are parity error ignored?

      Well, again i am not an expert in Windows COM PORT programming, but looking at the source code of BSL Scripter, especially BSL_IO_UART.c, if the target device is not the F543x non-A version, the initializeCommPort() function will initialize the COM PORT file with even parity. On the other hand, the readByte() function will just read out a byte from the COM PORT file. I am not 100% sure however if the COM PORT driver on Windows will check the parity according to the one which is set, but i think it should do.

      old_cow_yellow

      (d) I think the BSL code can choose to check or ignore parity bit. This is independent of whether they use Timer-UART or hardware-UART. For example,I know most F1xx and F2xx BSL use Timer-UART and they do check parity. You cited two actual BSL code, one ignores parity, the other one rejects bytes with parity-error.  What about other F5xx and F6xx?

      The code i cited above is basically taken from the SLAA450, the hardware UART BSL is taken from the CC430 one, while the timer UART is taken from the F5438A code. I am not sure about the older 1xx and 2xx code, since it has never been released publicly as the one for the 5xx/6xx ones.

      old_cow_yellow

      (e) What about FRAM chips and Wolverine?

      I am also not 100% sure about FRAM chips and Wolverine, since actually my privilege to the internal documentation is not so different as yours :) (considering i am just an application engineer whose main job is to give support to customers). However if i am not mistaken, in terms of protocol the BSL on FRAM devices should be considered similar with the Flash based BSL on 5xx/6xx devices altough on the FRAM devices the BSL resides in ROM (so unfortunatelly, no custom BSL possible).

      Hope this clears things a bit.

      Regards,

      Leo Hendrawan


      - Now that my signature has caught your attention, please click the "Verify Answer" button if this post answers your question. Thanks! -

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • old_cow_yellow
      Posted by old_cow_yellow
      on Jun 06 2012 15:38 PM
      Guru25715 points

      lhend
      ... I just tested another solution by using the MSP430G2553 with store and forward mechanism (with some delay addition in the BSL Scripter code) and it works also for the CC430 hardware UART BSL. The idea is to use Timer_A interface between PC and Launchpad (both working with 9600 baud and no parity), and USCI interface between Launchpad and MSP430 target (with 9600 baud, even parity). This should also work, but the BSL Scripter can not be used "as is" without any modification....

      How is this another solution doing?

      I just started my own version by using MSP430G2001 (or any MSP430G2xxx). It seems to work with the current BSL Scripter without any modification. However, it seems that the BSL Scripter has quite a few bugs and the old BSLDEMO2 does a much better job. I will need to do more tests to confirm my findings. I do not have all the various Targets to test. Are you interested in my G2001 version? Could you test it?

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Leo Hendrawan
      Posted by Leo Hendrawan
      on Jun 07 2012 02:25 AM
      Mastermind27025 points

      Hi OCY,

      old_cow_yellow

      How is this another solution doing?

      The solution works quite well, however i haven't tested to read large chunk of data from the MSP430 target. But at least for the test, it works quite well.

      old_cow_yellow

      I just started my own version by using MSP430G2001 (or any MSP430G2xxx). It seems to work with the current BSL Scripter without any modification. 

      How are you doing it? Have you tested to download/read out large chunk of data (for example downloading the Big_File.txt supplied in the SLAU319? The problem i was telling you is that the Launchpad is too slow for handling those kind of data. Would be interested of course to know how you design the Launchpad to bridge the data in this case.

      old_cow_yellow

      However, it seems that the BSL Scripter has quite a few bugs and the old BSLDEMO2 does a much better job. 

      Which bug do you mean? The most common bug for the BSL Scripter is that it won't work with USB Virtual COM PORT which is greater than 9. Well other "bugs" i know from BSL Scripter is that for example when you try to download a txt file but the file doesn't exist, it will just crash.

      old_cow_yellow

      I do not have all the various Targets to test. Are you interested in my G2001 version? Could you test it?

      Sure, but i won't be able to do it until the next two weeks. 

      Regards,

      Leo Hendrawan


      - Now that my signature has caught your attention, please click the "Verify Answer" button if this post answers your question. Thanks! -

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • old_cow_yellow
      Posted by old_cow_yellow
      on Jun 20 2012 23:41 PM
      Guru25715 points

      Leo,

      I was busy with something else too and did not get back to you about my implementation of this BSL Bridge.

      You said the Launchpad is too slow. But your code is using 1MHz and the Launchpad is capable of up to 16MHz. I set RSEL=13, DCO=3, and MOD=0 (~7MHz) and there is no need for hardware UART nor special version of PC software. I think it work fine.

      I have tested this with MSP430F1232, F135, F149, F2417, F5419A, and FR5739. I do not have anything else to test with. Can you find some time to try it?

      --OCY

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Leo Hendrawan
      Posted by Leo Hendrawan
      on Jun 21 2012 03:06 AM
      Mastermind27025 points

      Hi OCY,

      yes i implemented this only with 1 MHz because it works already with 1 MHz. Does it mean that you only change the clock setting the SLAA535 code or do you have any other changes?

      Regards,

      Leo Hendrawan


      - Now that my signature has caught your attention, please click the "Verify Answer" button if this post answers your question. Thanks! -

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • old_cow_yellow
      Posted by old_cow_yellow
      on Jun 21 2012 10:58 AM
      Guru25715 points

      Leo,

      No, I redesigned the entire thing. I think it works with any MSP430 member that has UART or Timer-UART BSL; but I cannot verify that.

      This is a summary of what it does:

      a) At power-up or SW1 generated reset, it drives Target nRST and TCK (if any) low, pulls up SW2, hold WDT, and wait a while for SW2 pull-up to work. It then waits for SW2 to be pushed. During this time, both green and red LEDs are off.

      b) When SW2 is pushed, it drives Target nRST, TCK, and TEST to invoke BSL Entry Sequence. As a result, the green LED is turned on because it is on the same signal line as TCK.

      c) If the Target recognized the BSL Entry Sequence, the red LED should also light up because it is on the same signal line as Target BSL TX.

      d) It speeds up the DCO to ~7MHz with no modulation and wait for PC TXD or Target BSL TX.

      e) It replicates PC-TXD and sends that to Target BSL-RX. But at the end of each byte, this replicate has the option to append an Even Parity Bit. It also replicates Target BSL-TX and sends that to PC_RXD.

      f) The first byte from PC-TXD is always 0x80. This is true for any ROM-Based BSL or Flash-based BSL. This is used to calculate the BAUD divider for ~7MHz DCO to get 9600 b/s.

      If you want, I can send you the entire code. It is in public domain.

      --OCY

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Leo Hendrawan
      Posted by Leo Hendrawan
      on Aug 07 2012 08:35 AM
      Mastermind27025 points

      Just to give an update,

      the SLAA535 has been updated http://www.ti.com/mcu/docs/litabsmultiplefilelist.tsp?sectionId=96&tabId=1502&literatureNumber=slaa535a&docCategoryId=1&familyId=342.

      The new version has been tested on various MSP430 device families ranging from 1xx, 2xx, 4xx, and 5xx family devices. including the CC430. I want to thank OCY for his contribution for this update.

      Regards,

      Leo Hendrawan


      - Now that my signature has caught your attention, please click the "Verify Answer" button if this post answers your question. Thanks! -

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Xiaohui Liu1
      Posted by Xiaohui Liu1
      on Nov 06 2012 17:23 PM
      Prodigy225 points

      Hi,

      I'm trying SLAA535 with this board. But the LPAD_BSL_INTERFACE project does not even compile. It shows a few errors during compilation:

      #20 identifier "TIMERA0_VECTOR" is undefined main.c /launchpad_bsl line 470 C/C++ Problem

      #20 identifier "TIMERA1_VECTOR" is undefined main.c /launchpad_bsl line 517 C/C++ Problem

      #20 identifier "USI_VECTOR" is undefined main.c /launchpad_bsl line 591 C/C++ Problem

      Can you please give me some hint on what may go wrong? Thanks.

      BTW, I'm using CCS 5.2.1.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Leo Hendrawan
      Posted by Leo Hendrawan
      on Nov 07 2012 02:49 AM
      Mastermind27025 points

      Hi,

      i guess you are using the MSP430G2553 on the Launchpad?

      If yes, you can use the source code which i posted here: http://e2e.ti.com/support/microcontrollers/msp43016-bit_ultra-low_power_mcus/f/166/p/209340/741073.aspx#741073

      Regards,

      Leo Hendrawan


      - Now that my signature has caught your attention, please click the "Verify Answer" button if this post answers your question. Thanks! -

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Xiaohui Liu1
      Posted by Xiaohui Liu1
      on Nov 07 2012 10:52 AM
      Prodigy225 points

      Hi,

      Yes, I'm using MSP430G2553.

      The code (3323.lpad_bsl_int_G2553.c) compiles now, but both LEDs blink, meaning the BSL invocation fails. Can you please advise where might go wrong? Thanks.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Leo Hendrawan
      Posted by Leo Hendrawan
      on Nov 07 2012 11:01 AM
      Mastermind27025 points

      Hi,

      since you are using a custom board, i would suggest to check for the connection. Have you connected the right pins of the MSP430F1611 on the custom board (RST, TCK, Data Transmit 13 - P1.1, Data Receive 22 - P2.2)?

      You need to push the reset button on the launchpad to try reconnecting with the BSL again.

      Regards,

      Leo Hendrawan


      - Now that my signature has caught your attention, please click the "Verify Answer" button if this post answers your question. Thanks! -

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Xiaohui Liu1
      Posted by Xiaohui Liu1
      on Nov 07 2012 12:10 PM
      Prodigy225 points

      Hi,

      You are right.

      My connection is below:

      MSP430G2553                  TelosB

      VCC                                     U2.1 (i.e., PIN 1 at expansion U2)

      GND (J6)                             U2.9

      P1.6                                     U2.4 (UART0TX)

      P1.7                                     U2.2 (UART0RX)

      P1.4                                     U28.6

      P1.0                                     U8.7 (i.e., pin 7 at JTAG)

      But actually, BSLTX is pin UART1TX and BSLRX is pin UART1RX, both are only found in I/O buffer. Is there anyway I cannot connect to these two pins (BSLTX and BSLRX) in my board? They are not in expansion pins nor JTAG.

      More information about my TelosB board is here. Thanks.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    12
    TI E2E™ Community
    • Support Forums
    • Blogs
    • Videos
    • Groups
    • Site Support & Feedback
    • Settings
    TI E2E™ Community Groups
    • TI University Program
    • Make the Switch
    • Microcontroller Projects
    • Motor Drive & Control
    Other Communities
    • Deyisupport
    • Designsomething.org
    • beagleboard.org
    • TI on Element 14
    • TI on TechXchangeSM
    Other Technical & Support Resources
    • WEBENCH® Design Center
    • Product Information Centers
    • Technical Documents
    • TI Design Network
    • TI Technical Articles
    • TI Training

    All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

    Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

    Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
    TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

    TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
    embedded processors, along with software, tools and the industry’s largest sales/support staff.

    © Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy Policy | Terms of Use