This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

MSP432P401R: ADC14 error for measured voltage in msp432

Part Number: MSP432P401R

Hi,

I am using a MSP432P401R Red Launchpad. I am trying to interface an LM35 temperature sensor with the controller and display the same over a K350 QVGA display. The LM35 is interfaced at P5.5 with ADC MEM15. 

The issue I am facing is that the microcontroller is unable to show the proper room temperature. The program I have writtten is working as desired sinceif the adc is fed with onboard 3.3 V supply, it shows 3300mV as output on the display. But on interfacing the same with LM35 gives weird output which is much higher or lower with respect to room temperature. Inorder to verify if the LM35 is working fine, I measured the output signal with DMM and it was showing 310 mV which is same to room temperature. But on interfacing it with msp432, the DMM reading keeps fluctuating around 160 mV and higher. Also an important thing i noticed is that when i measured the voltage at ADC channel i.e. P5.5, DMM gives reading of around 80mV and I guess its much greater that it should be.

Regards,

Amit Kotal 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.