This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/MSP430F5529: eZ-FET communication issue

Prodigy 20 points

Replies: 3

Views: 1666

Part Number: MSP430F5529

Tool/software: Linux

Hi everyone, I have been using the MSP430F5529 launchpad for a while now, however the ez-FET lite is now giving me some issues. I am using the back-channel UART that it provides to talk to my computer, this was working well until I changed from windows to Linux. Now the ez-FET gets stuck at random times where both the "power led" and the "mode led" turn on and the USB connectivity turns off. Looking at the datasheet for the ez-FET [1] this indicates that it is waiting for a data transfer, however we never consciously sent any information to the debugger, we only used the application UART. Any one know what are the reasons that could cause this error? I had a similar problem a while back due to a faulty voltage regulator sending trash over the serial line but it doesn't seem to be the case since i placed capacitors on the line to verify this. I am using the jetson-tx1 computer running an orbitty carrier board running linux 16.04.

Thanks, guys.

[1] ez-FET Datasheet: www.ti.com/.../slau647h.pdf

3 Replies

  • I am not a Linux/msp expert, but If there is (not disabled) modem manager, than it will try to (send some control bytes and) find a modem on any attached CDC device (including eZ-FET Lite back-channel UART).
  • Hi Jose,
    Please see Table 1 of the document you listed. The F5529 ez-FET is not compatible with Linux. You'll need to use a MSP-FET.

    Best regards,

    Cameron P. LaFollette

  • In reply to Cameron LaFollette:

    Cameron LaFollette
    The F5529 ez-FET is not compatible with Linux. You'll need to use a MSP-FET.

    Energia is working with F5529 eZ-FET Lite on Linux just fine.

    http://energia.nu/pin-maps/guide_msp430f5529launchpad/

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.