I'm using MSP430AFE253.
I want to send the conversion result from SD24 ADC (from MSP430AFE253) via SPI to an other MSP430F6638.
In the family data sheet MSP430AFE2x3, 3 modules are mentioned: USCI, USART and USI and all of them support SPI.
So what is the difference between this 3 modules?
In the data sheet of MSP430AFE253, only USART0 is mentioned. Does it mean that this device has only USART?
In the data sheet of MSP430F6638, only USCI is mentioned. Does it mean that this device has only USCI?
So if I build up a SPI communication between the 2 devices (AFE253 will be the master, and F6638 will be the slave), may any problem happen?
Thanks!