Hi, can someone help me out with a customer question? The customers question is as follows:
"If you take a look at page 5 of the MSP430AFE253 datasheet, the alternate functionality for pins 17 thru 20 are listed as follows:
17 SDCKL SD24_A bit stream clock output
18 SD0DO SD24_A bit stream data output for channel 0
19 SD1DO SD24_A bit stream data output for channel 1
20 SD2DO SD24_A bit stream data output for channel 2
The pin descriptions appear to point to a “built-in” raw A/D data streaming functionality. Unfortunately, it does not appear to be documented anywhere in the datasheet or user’s guide how to access this functionality. This is a functionality that we would possibly like to implement. I think at this point the question is more whether this was sort of an idea that didn’t end up being implemented in the device, or whether it is possibly new functionality that is implemented but is simply not yet documented. We did not find any code examples that appear to utilize the bit streaming functionality."
Any additional help or documentation on these alternate ppin functions that someone can provide would be tremendously appreciated! NOTE: my customer is planning to use the MSP430AFE253 device.