Hi.
Can not install demo-software on MSP-EXP430F5529 exp. board using CCS-size-limit v4.2.4 Have installed: 5529UE-1.10.01-setup and setup_CCS_MC_Core_4.2.400033 compile. I follow instruction in slau330a (3.3 Working With the Example Software) , selected CCS_Code_Size_Limit demo-software. USB connected to eZ-FET USB on board, led is green, jp16 selected all (default), power switch in mid pos: eZ.
When selecting "Debug active project" I get this error:
"MSP430: Trouble Writing Memory Block at 0x4400 on Page 0 of Length 0x386: This operation is not supported by this driver Cannot write to target."
The device manager show a new com port "MSP430 application UART" when connecting usb-cabel. Is this the right one.
Have reinstalled the devic-driver. Have searced this forum and tryed to follow sugestions, but that did not help.