I used Fet-Pro430 to reset the ez430-chronos to factory setting. After I did that, my wireless connectivity is not working? Is that got something to do with the 433, 868, 915 MHz source codes? I used the 915MHZ code for reset.
Thanks in anticipation,
Shailesh
Hi!
I'm facing the same situation.
First, I've tried to update my chronos's firmware thru wireless, but i've got an error message and it was impossible to try again. Then I opened the watch and made a wired download, using the debug interface and FET-Pro430 software.
After this I'm trying to comunicate in ACC mode and nothing happens. I see the AP's led flashing in a very low rate (1s on, 1 or 2s off) and the watch automatically ends the ACC mode. Did I do something wrong, during firmware download? I've used the following settings:
uController: CC-430F6137
Power: 3,3V
FIle: eZ430_Chronos_ Datalogger_915MHz_1_5.txt
I tried to erase only user memory, and then all memory.
Can someone help me with this situation?
(PS: My model is 915Mhz)
Thanks in advance!
Fernando Ginez da Silva
_________________________________