I can desing the ads1298 Register function to Impedance Meter desing?
Example product : MODEL 1089 MK III CHECKTRODE®
Various readings indicate the following:5 K or less – excellent skin prep: proceedwith recording and expect good results.5 – 10 K -- good skin prep, but expectsome noise in the recording.10 – 30 K -- fair skin prep. Contactimpedance may decrease with time, but forbest recording quality, electrodes should beremoved and skin re-prepped.Above 30 K -- bad skin prep. Even slightpatient motion will cause. Electrodes mustbe removed and skin re-prepped.
Yan Jia-hongI can desing the ads1298 Register function to Impedance Meter desing?
_____________________________________Before posting bug reports or ask for help, do at least quick scan over this article. It applies to any kind of problem reporting. On any forum. And/or look here.If you cannot discuss your problem in the public, feel free to start a private conversation: click on my name and then 'start conversation'. But please do so only if you really cannot do it in a public thread, as I usually read all threads. And I prefer to answer where others can profit from it (or contribute to it) too.