This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about circuit diagram of JTAG

Hello,

I am using a MSP430f2xxx series microcontroller... i wanted to know if there is any specific circuit diagram for the JTAG connection; i was browsing some websites where they have mentioned  pull ups on the TDI and TDO pins of the 4-wire JTAG connections.. is there any specific requirement for MSP430 devices? 

secondly, if the JTAG connector is not always hooked up to the JTAG pins, should the internal pull up or pull down resistors be enabled?

Can some1 plz help me?

thanks

4 Replies

  • Expert 1550 points

    You can find this information on the wiki:

    http://processors.wiki.ti.com/index.php/JTAG_%28MSP430%29

    That are only excerpts of hardware and user guides. Good starting point is here: http://www.ti.com/lit/ug/slau278h/slau278h.pdf

    --
    Regards,
    Jan

    Found any horrible English mistakes? - Drop me a note as private conversation via my profile if you like ;-)

  • In reply to Jan:

    I have checked that... it does not say anything about pull up or pull down resistors in any of the docs/... that's why i posted in forum

  • Expert 1550 points

    In reply to MSP430 Kors:

    As far as I remember this is exactly what is used on my boards, there are no additional parts. With SBW the resistor and more the capacitor on the reset pin need some care as SBW is a very fast serial protocol and the capacitor should not be too large.

    --
    Regards,
    Jan

    Found any horrible English mistakes? - Drop me a note as private conversation via my profile if you like ;-)

  • In reply to Jan:

    Jan
    With SBW the resistor and more the capacitor on the reset pin need some care as SBW is a very fast serial protocol and the capacitor should not be too large

    Alternatively, use a series resistor between RST pin and pullup resistor/pulldown capacitor). It significantly reduces the influence of the capacitor ont he SBW singal (which is tied directly to RST) but doesn't influence the effect of the capacitor for ensuring a safe startup on a slowly rising VCC (many cheap switching regulators, or a battery source that has to fill the buffer capacitors first etc). With a 1k series, you can easily use a 100nF capacitor, while without it, 2.2nF are specified as the maximum for SBW operation.

    _____________________________________

    Time to say goodbye - I don't have the time anymore to read and answer forum posts. See my bio for details.

    Before posting bug reports or ask for help, do at least quick scan over this article. It applies to any kind of problem reporting. On any forum. And/or look here.
    I'm sorry that  I can no longer provide help  in the forum or by private conversation.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.