We have been having problems debugging the MSPF5438 using IAR. We have a simple project set up with a timer running at 64Hz. If we try and put a breakpoint anywhere in the code, other then in the interrupt routine for the timer, the debugger always breaks at the interrupt and never where it should. This has become a very frustrating problem and is severly effecting the progress on our current project.
We are using the latest version of the IAR debugger / compiler connecting to a MSP-TS430PZ5X100 development board using a TI USB fet debugger. Does anyone have any ideas or suggestions on what could help us with this.
R