Has anybody successfully connected to an eZ430 using CCS5.2.0.00069 on Ubuntu 11.10 32-bit?
I have it installed and I have run install_script.sh using sudo.
When trying to run an example project using the supplied debug configuration I get the message
MSP430: Error initializing emulator: No USB FET was found
On investigation I found that the eZ430 is installing as /dev/ttyACM0 with owner - root, group - dialler and permissions - 660. I discovered that the removable device installation rule added by the install script to file /etc/udev/rules.d/61-msp430uif.rules is for a different device. I added another rule in file 61-ez430.rules as follows...
ATTRS{idVendor}=="0451",ATTRS{idProduct}=="f432",MODE="0666"
This is the same as the other rule but has the vendor and product IDs taken from the output of the lsusb command...
Bus 002 Device 017: ID 0451:f432 Texas Instruments, Inc. eZ430 Development Tool
Now the device installs with permission for anyone to read and write.
crw-rw-rw- 1 root dialout 166, 0 2012-06-05 12:41 /dev/ttyACM0
...but I still get the same error.
I've been trying to find a setting to set the device CCS uses to talk to the FET. I would have expected to find it in the Debug Configuration, but the CCS Device Debugging - Project launch configuration doesn't have Eclipse's usual Debugger settings.
Does anyone have some wisdom to share that might help?