MSP430 Pulse Oximeter
The project being developed is a pulse oximeter using an MSP430 and the LabView GUI available on ti.com.
Software available on Web helps run Microcontroller while under conditions of a certain application in this case the pulse oximeter.
The LabView GUI available on the Web, is supposed to producs output in the form of a waveform, but the waveform is not being displayed as output when running the GUI on the MSP430. Any suggestions on trouble shooting this issue?
The application notes are at this URL: