This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

development of a pulse oximeter using MSP430FG439 microcontroller

hi,

    my aim is to calculate oxygen saturation and heart rate.im using MSP430FG439 80-pin target board,which consists of pulse oximeter driver circuit and amplifier circuit.It has MSP430FET USB debugger with JTAG connector and USB port in target board.my doubt is how to interface spo2 sensor??that board consists of only JTAG and USB Port.

7 Replies

  • Gayathri Rajasekaran
    im using MSP430FG439 80-pin target board

    You mean this: http://www.ti.com/tool/msp-ts430pn80

     

  • In reply to Andy Neil:

    hi

       ya ...bt my kit is specially designed for pulse oximeter..

  • In reply to Gayathri Rajasekaran:

    So why didn't you design it (or get it designed) with the necessary connections for the sensor that you intend to use?!

    How can anyone answer questions about a "special design" without full details of that design?!

  • In reply to Andy Neil:

    i dint design its designed earlier by my college lab assistants....none of the students did project in tat particular kit..im trying to do bt i hav so many difficulties while debugging...i tried sample program ...output file(.out file) is generated bt stil i couldn't download the program...

                                                                                                                                                                                                                                                                                        regards.

                                                                                                                                                                                                                                                                                        Gayathri

                                                                                                                                                                                                                                                                            karunya university

  • In reply to Andy Neil:

    sir,

       initially i tried with the sample codes... after generating .out file also stil i couldn't download the program because of some debugging problems...

    pls check out the attachment....

    and my other doubt is how to interface the sensor???

  • In reply to Gayathri Rajasekaran:

    Gayathri Rajasekaran
    how to interface the sensor???

    How to interface anything: http://bit.ly/pWAASo

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.