I'm using the TrxEB (rev.1.7) which is equipped with the MSP430F5438A, and I'm using the CC1120 (rev.1.1) as radio. I would very much like to use an oscilloscope to measure how much current is used and to get a current profile so as to achieve greater insight into what steps/parts of my program is consuming the most current and why. I'm not very experience however with these practical matters so I'm wondering if anyone has an idea as to how I can achieve this? I know the TrxEB is equipped with 3 current measurement pin pairs, MCU_PWR, IO_PWR and RF_PWR. Can i simply connect one of these pin pair to an oscilloscope and that's that?