I am trying to achieve low current in LPM3 on a MSP430F5419a. I am running a small test app that enables 2 GPIO interrupts and the RTC Alarm interrupt then sets the GPIO pins for low power and enters LPM3 (with interrups enabled). The app flashes and LED several times when it wakes up to verify that the interrupts are working. With XT1 running on a 32k crystal and ACLK source XT1 the current in LPM3 is 6-7uA. If I don't enable the crystal and set ACLK source to VLO the LPM3 current is 2uA. With no crystal and ACLK source as REFO the LPM3 current is 5-6uA. We were expecting to - and are hoping to - acheive something like 2uA in LPM3 with the RTC running in crystal mode.