Hi,
I'm currently using the Real Time Clock on the MSP430F5438A and am having a few problems since updating to the V5.5 version of CCS. Unfortunately, this processor has some errata relating to the RTC which requires assembly functions (supplied by TI, pasted in below) to be used when reading from and writing to the RTC. I have attached the rtcASM.s43 which contains these functions.
With the latest version of CCS I am now getting some compiler warnings, which I cant remove, relating to the above module. Specifically:
Description Resource Path Location Type
[W0005] NOP required after set or rtcASM.s43 /transientMinderV3.0/src line 111 C/C++ Problem
[W0005] NOP required after set or rtcASM.s43 /transientMinderV3.0/src line 73 C/C++ Problem
[W0005] NOP required after set or rtcASM.s43 /transientMinderV3.0/src line 46 C/C++ Problem
[W0005] NOP required after set or rtcASM.s43 /transientMinderV3.0/src line 135 C/C++ Problem
[W0005] NOP required after set or rtcASM.s43 /transientMinderV3.0/src line 161 C/C++ Problem
[W0005] NOP required after set or rtcASM.s43 /transientMinderV3.0/src line 185 C/C++ Problem
[W0005] NOP required after set or rtcASM.s43 /transientMinderV3.0/src line 211 C/C++ Problem
With the exception of these warnings, my project compiles cleanly. As I don't have a detailed understanding of the exact errata issue being resolved by the assembly functions I do not feel confident editing it. I have tried disabling the warnings in the compiler but can't find the correct place to do so (tried --diag_suppress).
Any advice on either suppressing the warning or modifying the code would be gratefully received.
Many thanks
Ben Smither
;****************************************************************************** ; MSP430FG5438 - Real Time Clock Workaround ; ; Description: This program demonstrates the RTC Workaround for the RTC ; Errata deailed in the XMS '5438 Errata under RTC3 ; Assembly functions for the RTC workaround ; Allows safe access to the RTC registers that potentially have a write issue ; Code is aligned so that the lower 5 bits of the address of the instruction ; fetch following the RTC register write are equal ; Do not change the code in the ASM file (.s43) all nops in there are needed. ; ; Texas Instruments Inc. ; October 2008 ; Built with CCE version 3.2.2 ; ;******************************************************************************* ; !!!!!! Do not change the code. Every nop has a function !!!!!! ;******************************************************************************* .cdecls C,LIST,"msp430f5438Syrinix.h" ; Include device header file ;------------------------------------------------------------------------------- .text ; Progam Start ;------------------------------------------------------------------------------- .align 32 ;------------------------------------------------------------------------------- .global SetRTCYEAR ; int SetRTCYEAR(int year) ; year will be set in the RTCYEAR register ; return value is read back from the RTCYEAR register ; Works only in calendar mode (RTCMODE = 1) ; argument year is in R12 ; return value is in R12 SetRTCYEAR: nop nop nop nop dint nop nop nop mov.w R12,&RTCYEAR ; Set RTCYEAR to year nop nop mov.w &RTCYEAR,R12 ; Return value eint .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif ;------------------------------------------------------------------------------- .global SetRTCMON ; int SetRTCMON(int month) ; month will be set in the RTCMON register ; Workaround requires to write 16 bits into RTCDATE ; return value is read back from the RTCMON register ; argument month is in R12 ; return value is in R12 SetRTCMON: push.w R5 ; push R5 mov.b &RTCDAY,R5 ; read RTCDAY into R5 swpb R12 ; R12 holds month - swap lower and upper byte bis.w R12,R5 ; combine read RTCDAY and new RTCMON dint nop mov.w R5,&RTCDATE ; write to RTCDATE nop nop nop nop eint mov.b &RTCMON,R12 ; Read RTCMON register pop.w R5 ; pop R5 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif ;------------------------------------------------------------------------------- .global SetRTCDAY ; int SetRTCDAY(int day) ; day will be set in the RTCDAY register ; Workaround requires to write 16 bits into RTCDATE ; return value is read back from the RTCDAY register ; argument day is in R12 ; return value is in R12 nop nop nop nop nop nop nop nop nop nop nop nop SetRTCDAY: ; R12 holds day in lower byte push.w R5 ; push R5 mov.b &RTCMON,R5 ; read RTCMON into lower byte of R5 swpb R5 ; month is now in higher byte of R5 bic.w #00FFh,R5 ; clear lower byte of R5 bis.w R12,R5 ; combine read RTCDAY and new RTCMON dint nop mov.w R5,&RTCDATE ; write to RTCDATE nop eint mov.b &RTCDAY,R12 ; Read RTCDAY register pop.w R5 ; pop R5 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif ;------------------------------------------------------------------------------- .global SetRTCDOW ; int SetRTCDOW(int dow) ; dow will be set in the RTCDOW register ; Workaround requires to write 16 bits into RTCTIM1 ; return value is read back from the RTCDOW register ; argument dow is in R12 ; return value is in R12 SetRTCDOW: push.w R5 ; push R5 mov.b &RTCHOUR,R5 ; read RTCHOUR into R5 swpb R12 ; R12 holds dow - swap lower and upper byte bis.w R12, R5 ; combine read RTCHOUR and new RTCDOW dint nop mov.w R5,&RTCTIM1 ; write to RTCTIM1 nop eint mov.b &RTCDOW,R12 ; Read RTCDOW register pop.w R5 ; pop R5 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif ;------------------------------------------------------------------------------- .global SetRTCHOUR ; int SetRTCHOUR(int hour) ; hour will be set in the RTCHOUR register ; Workaround requires to write 16 bits into RTCTIM1 ; return value is read back from the RTCHOUR register ; argument hour is in R12 ; return value is in R12 SetRTCHOUR: ; R12 holds day in lower byte push.w R5 ; push R5 mov.b &RTCDOW,R5 ; read RTCDOW into lower byte of R5 swpb R5 ; dow is now in higher byte of R5 bis.w R12,R5 ; combine read RTCDOW and new RTCHOUR dint nop nop mov.w R5,&RTCTIM1 ; write to RTCTIM1 nop eint mov.b &RTCHOUR,R12 ; Read RTCHOUR register pop.w R5 ; pop R5 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif ;------------------------------------------------------------------------------- .global SetRTCMIN ; int SetRTCMIN(int min) ; min will be set in the RTCMIN register ; Workaround requires to write 16 bits into RTCTIM0 ; return value is read back from the RTCDOW register ; argument min is in R12 ; return value is in R12 SetRTCMIN: push.w R5 ; push R5 mov.b &RTCSEC, R5 ; read RTCSEC into R5 swpb R12 ; R12 holds min - swap lower and upper byte bis.w R12,R5 ; combine read RTCMIN and new RTCSEC dint nop mov.w R5,&RTCTIM0 ; write to RTCTIM0 nop eint mov.b &RTCMIN,R12 ; Read RTCDOW register pop.w R5 ; pop R5 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif ;------------------------------------------------------------------------------- .global SetRTCSEC ; int SetRTCSEC(int sec) ; sec will be set in the RTCSEC register ; Workaround requires to write 16 bits into RTCTIM0 ; return value is read back from the RTCSEC register ; argument sec is in R12 ; return value is in R12 SetRTCSEC: ; R12 holds day in lower byte push.w R5 ; push R5 mov.b &RTCMIN, R5 ; read RTCMIN into lower byte of R5 swpb R5 ; min is now in higher byte of R5 bis.w R12, R5 ; combine read RTCMIN and new RTCSEC dint nop nop mov.w R5,&RTCTIM0 ; write to RTCTIM0 nop eint mov.b &RTCSEC, R12 ; Read RTCSEC register pop.w R5 ; pop R5 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif ;------------------------------------------------------------------------------- .global GetRTCTIM0 ; Read the RTC registers RTCTIM0 ; return the values GetRTCTIM0: mov.w &RTCTIM0,R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCTIM1 ; Read the RTC register RTCTIM1 ; return the values GetRTCTIM1: mov.w &RTCTIM1,R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCDATE ; Read the RTC register RTCDATE ; return the values GetRTCDATE: mov.w &RTCDATE,R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCYEAR ; Read the RTC registers RTCYEAR ; return the values GetRTCYEAR: mov.w &RTCYEAR, R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCMON ; Read the RTC register RTCMON ; return the values GetRTCMON: mov.b &RTCMON, R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCDOW ; Read the RTC register RTCDOW ; return the values GetRTCDOW: mov.b &RTCDOW, R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCDAY ; Read the RTC register RTCDOW ; return the values GetRTCDAY: mov.b &RTCDAY, R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCHOUR ; Read the RTC register RTCDOW ; return the values GetRTCHOUR: mov.b &RTCHOUR, R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCMIN ; Read the RTC register RTCDOW ; return the values GetRTCMIN: mov.b &RTCMIN, R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif .global GetRTCSEC ; Read the RTC register RTCDOW ; return the values GetRTCSEC: mov.b &RTCSEC, R12 .if $isdefed("__LARGE_CODE_MODEL__") = 0 ret .else reta .endif