My goal right now is to have a push button trigger an interrupt to turn on the LED for a certain period of time. So I need a timer to shut off the LED once the timer has ran to 0. For some reason my code works like planned in debug mode on CCS, but when I get off debug mode it doesn't work. It seems like the timer interrupt is never called. I am using TIMER0_A0 which I believes clears the source of the interrupt by itself.
Does anyone know what flag I would have reset for this type of timer?
This makes it very frustrating to debug because I can't step through the code.
If any wants to see the code I can provide my program, which is pretty short.