I am using CCS v5.4.0.00091 for the MSP430FR5739.
I am using Grace to define Timer0_B3, Timer1_B3, and Timer2_B3 for PWM outputs.
CCS is forcing Timer0_A3, and Timer1_A3 into the compile adding the error, "Timer1_A3" is not defined.
I cannot remove the *_A3 timers as they are locked on the main.cfg peripheral list.
What can I do to remove the *_A3 Timers so that I can compile my code.
Thanks.