I have a new project for the FRAM Wolverine MSP430FR5969. The project compiles without errors or warnings but when I click on Debug it loads the code to the micro and immediately starts running the code instead of stopping at main so I can single step. If I then click on Pause it complains it cannot find the source:
Can't find a source file at "/tmp/TI_MKLIBeR36VQ/SRC/copy_decompress_rle.c"
Locate the file or edit the source lookup path to include its location.
I have "run to main" selected. This is a new project that I started from scratch so I probably just have something set up wrong.
ideas welcome!