HI
My external AD-converter generates data ready interrupt on p1.0 After interrupt I read the conversation result over SPI. I am trying to use DMA1 and DMA2 on SPI transmission. DMA1 is triggered on USC1A0RXIFG and DMA2 on USCIA0TXIFG. DMA1 generates a DMA interrupt when ready.
My problem is that DMA interrupt isn't genrated when I keep p1.0 interrupt always enabled. If I disable the p1.0 interrupt on P1IE until dma interrupt is generated everything works fine on MCU but there will be issues on AD-converter.
Is there any limitations on MCU that I should know or is it just my code? I also tried to replace DMA1 with DMA0 without any good results.