Having a USB issue with the MSP430F5510. When we try to download an upgrade to the flash memory, the MSP430F5510 does not respond. We are using the default BSL and clocking at 4 MHz. We have 20 boards, 6 boards work fine, the other 14 do not. We have checked the hardware to make sure the clocks are working, the power is working, and that there is no cross talk or noise on the input traces. When we try tracing the issue with the debugger, everything looks normal until the code transfers control to the BSL. Then we can no longer track the code.
Has anyone out there encountered an problem similar to this or have any suggestions on how to continue de-bugging?
Thanks,
Chuck