Hello,
i want to use this device to measure rated currents of 1A, 2A, 5A and 10A.
In the Apllication Report (http://www.ti.com/lit/an/slaa577e/slaa577e.pdf) the EVM430 is used with CTs. Most CTs i find are specified for rated currents of 30A or above. So is it also possible to use a simple shunt instead of the CT?
In another post ive seen that CTs are already included in the package. (http://e2e.ti.com/support/microcontrollers/msp430/f/166/t/334379.aspx) Is that true? And where do i get the specifications of these CTs?
Thank you