Dear USB Users,
A new release of USB Developers Package 4.10.02 is now available from:
Please note that this release may be used with CCS 5.5 but if GCC functionality is required, CCS 6.0 should be used. CCS 6.0 is currently only available as a beta version.
New in USB 4.10.02
- USB stack code and examples updated with compiler define DRIVERLIB_LEGACY_MODE for backward compatibility with driverlib.
- Python Firmware Upgrader tool updated with RAM_BSL.00.07.88.38.txt file
- MSP430 USB Firmware Upgrade Example tool updated with RAM_BSL.00.07.88.38.txt file
- MSP430 USB Firmware Upgrade Example tool updated to close all open files correctly.
- Updated types.h file with the removal of existing structure definitions
- SYSBIOS examples updated to remove warnings seen in IAR