I have following two utilities to upgrade the MSP430 firmware.
1. MSP430 USB Firmware Upgrade Example v1.3.0
2. MSP430 USB Firmware Upgrade Example 2.0
With both of these utilities, it is only possible to upgrade the firmware using CMD no: 18 (Mass erase) but our aim is to use CMD 16: (Erase segment) for upgrading the firmware as I do not want to upgrade information memory each time. Following are our concerns:
1. MSP430 USB Firmware Upgrade Example v1.3.0 (on Visual Studio)
I took the TI code and tried to build it. It gave following error
Error 30 error LNK1181: cannot open input file 'hidparse.lib' D:\SourceCode\BSL430_DLL\LINK BSL430_DLL
With this error I are not able to proceed to check if I can really use CMD 16.
2. Python_Firmware_UpgraderGUI.exe (MSP430 USB Firmware Upgrade Example 2.0) at ‘C:\ti\msp430\MSP430ware_1_60_02_09\usblib430\Host_USB_Software\Python_Firmware_Upgrader’
Here also only CMD 18 is used. I need your support to change the python file because I don’t have any expertise.
Can you please guide me, how can we proceed OR can TI provide some utility to upgrade FW using CMD 16?