Hello,
I recently purchased a MSP-EXP430F5529LP (LaunchPad eval board with MSP430F5529) and have not been able to program it through CCS. Additionally, the demo program that is supposed to run (according to the quick-start guide) does not show up in any form.
I've read several posts regarding similar issues but have not been able to resolve my problem with the suggested solutions.
Here are a few pieces of information that might help determine what the issue is:
1) I've tried with CCS 5.4, 5.5, and 6.0, each time completely uninstalling any other versions
2) I'm running Windows 7 x64
3) When I first plugged the board in, windows installed drivers, but only for "HID-compliant device" and "USB Input Device"
4) It is listed in device manager as "Generic USB Hub"
5) It shows up as two "USB Input Devices" in my control panel's 'Devices and Printers'
6) I have a MSP-EXP430G2 LaunchPad and it has worked correctly the whole time (i.e. it shows up as a TI MSP430 device and I am able to program it through CCS)
7) The device ID (according to USB Device Tree Viewer) is "USB\VID_2047&PID_0200"
8) I've tried plugging it into several different USB ports with no change to the problem
One of the other posts I read (http://e2e.ti.com/support/microcontrollers/msp430/f/166/t/296908.aspx) suggested that it may just be a faulty board, but I wanted to get some more opinions before I go that direction.
Best regards,
Anthony