Hi,
I'm trying to flash MSP430F5529 from commands line via JTAG and at the end I've got Exit 16 and Error: unknown device.
Do I use wrong arguments or it's flasher bug? (by the way, CCS6 flashing works just fine).
Full log:
C:\ti\MSP430Flasher_1.3.1>MSP430Flasher.exe -n MSP430F5529 -m JTAG -w "firmware.hex" -v -g -z [VCC] * -----/|-------------------------------------------------------------------- * * / |__ * * /_ / MSP430 Flasher v1.3.1 * * | / * * -----|/-------------------------------------------------------------------- * * Evaluating triggers...done * Checking for available FET debuggers: * Found USB FET @ COM13. <- Selected * Initializing interface @ COM13...done * Checking firmware compatibility: * The firmware of your FET is outdated. - Would you like to update it? (Y/N): y * ********************************************************* * ********************************************************* * * * * Initializing Update Bootloader. * * Erasing firmware memory section. * * Programming new firmware: * * Exit Update Bootlader and reboot firmware. * ********************************************************* * ********************************************************* * * * * Initializing Update Bootloader. * * Erasing firmware memory section. * * Programming new firmware: * * |||||||||||||||||||||||||||||||||||||||||||||||||| 100% * * Exit Update Bootlader and reboot firmware. * * Update was successfully finished. * * * ********************************************************* * ********************************************************* * FET firmware is up to date. * Reading FW version...done * Reading HW version...done * Setting VCC to 3000 mV...done * Configuring...done * Accessing device... # Exit: 16 # ERROR: Unknown device * ---------------------------------------------------------------------------- * ERROR on close: No error * ---------------------------------------------------------------------------- */ C:\ti\MSP430Flasher_1.3.1>
Regards,
Alexey