L.S.,
On a MSP430G2553 I need to be able to inhibit a TI PTH08080W from software. To do so, I thought to connect a GPIO port (1.5 in my case) to ground, by setting it to input and pulldown. According to the datasheet (p. 24), the internal pulldown resistor value is 20k - 50k. However, when I connect pin 5 of the PTH08080W to GPIO1.5, no inhibition is seen.
On the other hand, if I manually connect the inhibition pin to ground through a 100k resistor, it works, so the pulldown resistor value should not be the issue. I was under the impression the GPIO ports could sink current,
What am I missing? Thanks in advance!