I am using the EXP430FR5739. I have been flashing and running code on it for about 6 months now. All of a sudden, with no tinkering to hardware, I had an error when flashing software. I don't remember it exactly, but I think it said something to the effect of that the program .out file was corrupt. Now, I can't flash it again. The error message I get is: Error connecting to the target:
Could not find device (or device not supported)
Is there anyway to get it working again?
I would assume no if I were programming right to the FRAM chip via JTAG, but since it looks like the program is going through another MSP430 and getting flashed onto the FRAM chip from the other MSP430, I thought there might be something that could be done to save this board.
Thanks for your help.