hello,
I have searched information on MSP430 target type identification in the forum but I can't find what I need:
http://e2e.ti.com/support/microcontrollers/msp430/f/166/p/206507/732240.aspx#732240
http://e2e.ti.com/support/microcontrollers/msp430/f/166/p/87094/300954.aspx#300954
I would like to identify my target in my code to be able to have one version of the code running on several target and PCB.
is it possible to identify the target? (for me, it is between F2619 and F2618).
I checked the memory on 0x0FF0 zone like explained on several topics, I have exactly the same value for both target type. and the code is not explained.
the FET debugger is able to know which target is present so it should be possible to it also in the code.
thanks for your help.