I am designing an ultra low power device that wakes up from standby mode every 1 minute, measures from sensor and goes to standby again. The device is working with internal batteries. For selecting a processor, I have reached to the point of selection between MSP430F5x and RL78/G13.
512KB Flash RAM and 32KB SRAM of RL78/G13 (against 256KB Flash and 16KB SRAM of MSP430) as well as its lower active mode power consumption (66uA/MHz vs 23- uA/MHz) is tempting for our device. However, the extended temperature range (-55C) as well as more flexible clock system of MSP430F5x is tempting for me as well.
I have to mention that I have not done any measurement to compare the power consumptions and I have studied only the datasheets, however, I cannot rely only on the numbers in datasheet. Regardless of the Flash memory size and extended temperature rand, could you please help me to have a comparison between the power consumption of MSP430F5x and RL78/G13.
Thanks