Hii....
i am making a project in which i am using two microcontrollers msp430g2553
i want to make a serial communication between these two microcontrollers.
The theoretical explanation of project
From first microcontroller i want to transmitt "A" through serial port to the 2nd microcontroller ,it will receive via RxD pin the letter "A" and compares it with already stored "A" letter at different memory address .if the data received by 2nd microcontroller matches with the data already stored then i want to glow a green LED via port 1.6 and if data received doesnt matches then a red LED shld glow via port 1.0
can anybody help me with the coding of this problem
baud rate is to be 9600