Hi:
I've been trying to send data via UART to the computer with the application board MSP-EXP430F5529. The problem arises when I want to send several data one after another (numbers). What I normally do is:
1. Wait for the TX-Buffer to be ready
2. I send the data writting on the buffer
3. I wait for a DELAY of 1000 cycles
4. Repeat step 1 for sending the next byte
The problem is only that I I really think it is not optimum to put that DELAY of step 3, but if I don't do it, I receive strange characters (I check with a serial monitor). What should I do?
Thanks!