I am using an msp430f5328 and want to utilize ADC with the built-in temperature sensor for my application. However, it seems I have found a discrepancy, and I am hoping someone can help clear up my confusion.
It says in the MSP430x5xx and MSP430x6xx Users Guide that the built-in temperature sensor must have a sampling period of 30us, but then in the Data Sheet is says that the sample time required is at a minimum of 100us. My assumption is to follow the data sheet is specific to this particular board. Am I right in my assumption?
Secondly, does this 100us mean I have to set my sample-hold time to 512 cycles (Using the internal 5MHz sampling clock on the board, resulting in 102.4us), or can I simply turn the board on, wait for 100us, and then start sampling the sensor at a lower sample-hold time?